Part Number: TPS1663
We are using TPS16630RGER efuse in one of the circuits which sources power to other secondaries. Attached is the snapshot from schematics. The load connected to it is secondaries (DC:DC converts, MCU LDOs, comparators, etc) and…
Part Number: TPS1663 Hi team,
Regarding the TPS1663, the datasheet does not explicitly describe the recommended handling for an unused OVP pin, so I would like to confirm the following.
My understanding is that the OVP pin is the input to a comparator…
Part Number: TPS1663 Other Parts Discussed in Thread: TPS2663 , , TPS1653 Hi,
The TPS1653/TPS1663/TPS2663 e-fuses all have a dv/dt inrush control, and thermal regulation if there is an excessive current (for example short circuit) during startup? But…
Part Number: TPS1663 Hi all,
I would like to ask some questions about the TPS16630PWPT eFuse.
Could you please provide information regarding its operation and protection behavior?
After an overvoltage condition is detected by the TPS16630, is the…
Part Number: TPS1663 Dear
In my design, I use tps16632 to deisgn the 30V power output. In the design, I(OL) is 6A. From the datasheet, I(FASTRIP) =2xI(OL)=12A, I(SCP)=45A.
From the datasheet, I find the response time when output short happens as…
Part Number: TPS1663 Dear Team,
My customer is evaluating the TPS16630RGER in their application, and measured unpexpected /FLT output under the overload protection test.
TPS16630RGER settings: - VIN: 24V - UVLO pullup to IN1/IN2/P_IN - OVP pulldown…
Part Number: TPS1663 Hellow,
On the TPS16630 device, If the device has MODE pin in the open position set to have the device latch off in a fault condition, does that also apply to if the SHDN pin is pulled low?
Thanks, Zack
Part Number: TPS1663 Tool/software: Hi as per the evaluation board schematics of TPS1663 pin number 19 (NC-highlighted in image) is connected to output.
Is it ok of i connect this pin 19 to ground? or is there any issues doing so?
Regards
Sooraj…
Part Number: TPS1663 Dear Texas Instruments Support Team,
I hope this message finds you well.
I am currently evaluating the TPS16630PWPT device for a power distribution application and would like to clarify a couple of points regarding its operation…