Part Number: TPS1663 Tool/software: Hi as per the evaluation board schematics of TPS1663 pin number 19 (NC-highlighted in image) is connected to output.
Is it ok of i connect this pin 19 to ground? or is there any issues doing so?
Regards
Sooraj…
Part Number: TPS1663 Other Parts Discussed in Thread: LM76202-Q1 Tool/software: Dear Support, We need a similar TPS1663 chip, but automotive grade.
Thank you in advance
Antonio
Part Number: TPS1663 Tool/software: Hi Team,
Is it absolutely necessary to include a TVS diode on the IN pin of the TPS16630? We are currently designing a circuit using the TPS16630. I'm supplying a rated 24V power source to the IN pin. However, I observed…
Part Number: TPS1663 Tool/software: Hi
I have below questions on TPS16632.
1. If mode pin is grounded, will the device be working on auto retry mode during a output direct short to ground?
2. Should i keep the SHDN pin grounded or floating? if i…
Part Number: TPS1663 Tool/software: Hi, TI expert
A customer has requested a circuit review of TPS1663 applied.
Please check if there are any parts to be modified or added.
POE+SWITCH_SCH_REVIEW.pdf
Please check. Thank you.
Part Number: TPS1663 Other Parts Discussed in Thread: TPS2663 Tool/software: Hi Team,
We would like to know is there any way to simulate this efuse circuit?
whether through webench it is possible?
Regards, Sathya Priya N.
Part Number: TPS1663 Other Parts Discussed in Thread: TPS2663 , TPS1686 Tool/software: Hi Team,
We need to include reverse protection circuit with input range from 10V to 30V and output current limit will more than 7A, could you please suggest alternate…
Part Number: TPS1663 Tool/software: Hello E2E Experts,
Good day.
Can you also please do a general circuit review?
System details for context
Source: 24 V, 20 A max AGM battery, alternator‑charged; ISO 7637 & ISO 16750 transients mitigated…
Part Number: TPS1663 Tool/software: Hi Team,
I have a technical question about TPS16330 component configuration.
In one of the designs I have seen the OVP pin to GND.
I could not locate in the datasheet an explanation of what is the OVP threshold…
Part Number: TPS1663 Tool/software: Dear TI Team,
I would like to clearify the minimum needed output capacity for the TPS16632.
In the datasheet I can find a number of 100nF.
But the excel calculator states that we need 1050µF.
I hope this…