Part Number: TPS1685 Hello,
The datasheet for the TPS16850 references a PG de-glitch time, tPGA and tPGD. However I do not see these defined in the datasheet with actual numbers. What are these de-glitch times, in units of us, ms, etc.?
Part Number: TPS1685-CALC Hi, Some time ago I asked a question related to TPS1785 simulation model issues : TPS1685-CALC: TPS1685 simulation issues - Power management forum - Power management - TI E2E support forums Is the new simulation model available…
Part Number: TPS1685 Would you kindly assist with reviewing the issue I raised earlier?
: TPS1685: TPS16850(auto-retry) Slow OC behavior - Power management forum - Power management - TI E2E support forums
Part Number: TPS1685 Other Parts Discussed in Thread: TPS1689 My design consists of two TPS16851 in stacked configuration. They are managing the power going to two robotic arms. Each arm uses 15 amps of 24 V at peak, so two arms use 30 amps at peak. When…
Part Number: TPS1685-CALC Other Parts Discussed in Thread: TPS1685 Hi, I'm trying to simulate an application with TPS1685 but it is not working properly. I'm starting the simulation with only a 10uF capacitor as load, after the efuse is started I'm adding…
Part Number: TPS1685 Hi, when using multiple TPS1685x in parallel:
Is it possible to connect all !FLT pins together to one pull-up resistor? Or would it be adequate to use the primary-fuse !FLT output only?
Is it neccessary to connect all PGOOD…
Part Number: TPS1685 Hi, we are currently testing the TPS1685x as an E-Fuse for our new design. We need a fuse operating at 48V with 20A continuous current and no "current regulation" (limiting current while Iout>20A). It should trigger a fault after…
Part Number: TPS1685 I have an application using the TPS1685 as a resettable fuse. It appears that the device can never start if a load takes 2A or greater as the device enables its output due to ISFT(SAT) being 2A - is this interpretation correct?
Part Number: TPS1685 Hi,
I am having trouble getting the TPS16851 to startup at voltage 60V or higher (Cout = 470uF and No load). With the same setup, 59V or below it worked correctly.
I tried to increase the startup time with Cdvdt upto 1uF to keep…