Part Number: TPS1685 Tool/software: Hello,
In using the TPS16580 in standalone mode - how can the internal current reference for IREF be disabled so that pin can be driven by a DAC?
Thanks, John
Part Number: TPS1685 Tool/software: Hello,
I can't find information about the TPS1685 when there is a regenerative current (motor drive application) flowing from the output to the input during short period of time.
Does the IMON,ILIM continue to work…
Part Number: TPS1685 Tool/software: We are looking for an in-rush current controller like LM5069MM−2/NOPB but that does not use Vin as an input sense.
I would like to have the Vdd for the chip a voltage (9-20V) not related to the Rsns (IN) voltage…
Part Number: TPS1685 Tool/software: Hello,
Could you provide some spec (even preliminary) in order to determine the maximum output capacitor.
A Cauer thermal model would be ideal.
Thanks
Part Number: TPS1685 Tool/software: Hey team,
If I wanted the device to trip at 18A, but did not want fast-trip or overcurrent protection enabled, would I tie ILIM to a resistor and IMON to GND and IREF open?
Page 34 says that if ILIM / IMON are GND…
Part Number: TPS1685 Tool/software: Hi team,
As title, what's the difference between these 2 parameter? And when those parameters are involved?
Another quesion, if we use two phase, the start up current is about 1.1A(0.56A*2). Right?
Thanks,
Ol…
Part Number: TPS1685 Tool/software: Hello,
Re-asking again because my previous message was not answered and the thread is blocked. The datasheet shows individual resistors for SFT_SEL but the EVM shows one resistor for all devices.
The internal current…