Part Number: TPS1H200A-Q1 Hi Experts,
TPS1H200A-Q1 is under evaluation on customer side. There are several issues occur on customer side, could you help on those issue? Thanks.
When the device is Latch-off mode, when the overcurrent occurs, it takes…
Part Number: TPS1H200A-Q1 Hi team,
My customer are using TPS1H200 HSD in our project, I have some question regarding the diagnostic.
From below table, after DIAG_EN pin is enabled,
Pin IN, we can control by our IOC;
Fault Pin: we can read out by our I…
Part Number: TPS1H200A-Q1 Hi,
what is the maximum current limit threshold that TPS1H200A can offer with external resistor? for example, can i set it to 10A if i use an external resistor ? Thank you!
Part Number: TPS1H200A-Q1
Why does the Fault signal occur when the current swings as shown in the above result for the TPS1H200A-Q1 IC?
Is it because of current limit exceed due to inrush current?
There is no information in the datasheet. What could…
Part Number: TPS1H200A-Q1 Any idea what the resistance from OUT to GND should measure when the device is unpowered? Customer is trying to make some quick checks of the device mounted on their board and measure 7k ohms under this condition and are trying…
Part Number: TPS1H200A-Q1 Hi,
I need LT SPICE Model for the part TPS1H200A-Q1.Could it be provided. Else, can you please suggest a similar part.
Regards,
Reshma
Part Number: TPS1H200A-Q1 Hi,
I have one question regarding TPS1H200A, it cmalps Vds when negative voltage happens which is different with my understanding. i often use a free-wheel diode inparallel with my inductive load, thus OUT will be clamped -0…
Part Number: TPS1H200A-Q1 Hi team,
I have several questions and request.
"7.3.5.2.1 Output on" describes the contents of the fault detection function when Output=on. I would like you to develop an image diagram in the circuit to see where overcurrent…
Part Number: TPS1H200A-Q1 Hi,
I am now evaluating TPS1H200A for my new project. when i test this part, i found one abnormal behavior.
I connected DEALY pin to VS through 100K resistor. CL pin to ground to use internal current limit. then i draw 6A current…
Part Number: TPS1H200A-Q1 Hi,
in the datasheet, the hic(on) time is 40ms, and hic(off) is 1s. but when i tested TPS1H200A, i found a 80ms time. then output current keeps 0A for 1s, then back to 40ms current limit.
Can you please help to explain why there…