Part Number: TPS1HA08-Q1 Hello, we want to use TPS1HA08C as Power Switch to supply a number of ECUs. We do not know, which electronics might be connected to this Power Switch in the future, so we need to define limits for Capacitance / Current Draw.
I could…
Part Number: TPS1HA08-Q1 Hi team,
When EN=L and DIA_EN=H, will the normal current sense function work even if the FET in the IPD is broken by short then the VBB-VOUT is short-circuited?
Regards,
Youhei MIYAOKA
Part Number: TPS1HA08-Q1 Hi Experts,
For TPS1HA08-Q1, Is ICL (current limit) fixed or can we change based on load demands? If in case Current limit is fixed? Please suggest an help suggest an alternative.
Thank you and best regards,
Gerald
Part Number: TPS1HA08-Q1 Hi team,
Could you advise all the affected parameters and its impact if VBB is above 3V but less than 8V?
It is explained in the datasheet as below. It seems R ON is small increased. Is there any other parameters or functions that…
Part Number: TPS1HA08-Q1 Other Parts Discussed in Thread: TPS3305 My two questions are about the differences between version A and version E of the device
We have an existing circuit whose design includes version A — so, the full device number is TPS1HA08A…
Part Number: TPS1HA08-Q1 Hi team,
Could you advise the difference between I SB and I OUT(standby) current in the EE table of the datasheet?
I would like to know the total input current drawn from battery (12V lead acid battery connected to VBB) in stanby…
Part Number: TPS1HA08-Q1 Hi Expert,
I see that TPS1HA08-Q1 has energy limit. So I just link it to I2T function in eFuse application. I suppose they are not the same but I don't know what's different. May you help clarify? Thanks.
BR,
Elec Chen…
Part Number: TPS1HA08-Q1 Dear team,
Could you please tell me the difference between energy limit and thermal shutdown? I think these two functions are same, so I don't understand why we add energy limit function here?
Thanks & Best Regards,
S…
Part Number: TMUX582F-SEP Other Parts Discussed in Thread: SN74HCS238 , SN74AHC238 , TPS27SA08 , TPS1HB08-Q1 , TPS2HCS10-Q1 , TPS1HA08-Q1 Tool/software: The part I entered above is not the right one. I just put it there to get past the Required Field requirement…