Part Number: TPS1HA08-Q1 Hi team,
Our customer will usTPS1HA08 to their project.
The customer wants to turn off the enable pin at load current.
I think it's no problem, but please let me know if there is anything you need to be aware of.
Best Regards…
Part Number: TPS1HA08-Q1 Team - question from my customer below:
"We would like to understand how the LATCH Pin works in TPS1HA08B-Q1.
Actually our idea is to use only two lines from the controller i.e. EN and LATCH to FET.
We are not preferring…
Part Number: TPS1HA08-Q1 Hi team,
I see that the datasheet of TPS1HA08 does not provide the spec of the response time of over-current and over-temperature time, could you help provide such information?
Thanks!
Jayden Li
Part Number: TPS1HA08-Q1 Hi, I am using TPS1HA08-Q1, and I don't understand the input characteristics of EN pin.
①I do know that If the device is off and want it to go on then the voltage of the pin has to go to V IH, EN 2.0V ,if the device is on and…
Part Number: TPS1HA08-Q1 Other Parts Discussed in Thread: TPS1HB08-Q1 , Hi team,
Is there clamp circuit for EN pin?
TPS1HA08-Q1 and TPS1HB08-Q1 says recommended Enable voltage is under 5.5V. If it has clamp diode for EN pin, is it possible to use 12V input…
Part Number: TPS1HA08-Q1 Other Parts Discussed in Thread: TPS1HB08-Q1 , , TPS27SA08 Hello team,
I want some get recommendation of devices for the below requirements.
Nominal current : 5A
Current limit : 20A
Could you give me some recommendation of HSS(1ch…
Part Number: TPS1HA08-Q1 Other Parts Discussed in Thread: TPS1H100-Q1 , HSS-MOTHERBOARDEVM Always I am indebted.
My name is Mitsubishi Electric engineering Tanabe.
I have a question about the subject.
Currently, we are confirming the function of TPS1HA08CQPWPRQ1…
Part Number: TPS1HA08-Q1
Hello.
I would like to use 23.1V ~ 29.4V battery power to drive the motor.
I want to connect this battery power directly to the motor's controller power.
In other words, I want to use the TPS1HA08-Q1 to turn on/off the 24V…
Part Number: TPS1HA08-Q1 Hi,
We are using a FET switch TPS1HA08AQPWPRQ1 on our board for controlling "PERI_VIN_12V0" power supply. This FET switch is enabled by slide switch SW29.
Case1:When we turn ON the switch SW29 we are getting 12V…