Part Number: TPS1HA08-Q1 Other Parts Discussed in Thread: TPS1H100-Q1 , HSS-MOTHERBOARDEVM Always I am indebted.
My name is Mitsubishi Electric engineering Tanabe.
I have a question about the subject.
Currently, we are confirming the function of TPS1HA08CQPWPRQ1…
Part Number: TPS1HA08-Q1
Hello.
I would like to use 23.1V ~ 29.4V battery power to drive the motor.
I want to connect this battery power directly to the motor's controller power.
In other words, I want to use the TPS1HA08-Q1 to turn on/off the 24V…
Part Number: TPS1HA08-Q1 Hi,
We are using a FET switch TPS1HA08AQPWPRQ1 on our board for controlling "PERI_VIN_12V0" power supply. This FET switch is enabled by slide switch SW29.
Case1:When we turn ON the switch SW29 we are getting 12V…
Part Number: TPS1HA08-Q1 Hi Experts:
My customer is evaluating the device's behavior in the various input voltage. The typical input is 12V , but the minimum value could be approaching 7V voltage,
as the description of the datasheet like below, the…
Part Number: HSS-MOTHERBOARDEVM Other Parts Discussed in Thread: TPS2HB08-Q1 , TPS27SA08 , TPS2HB35-Q1 , TPS2HB50-Q1 , TPS1HA08-Q1 , TPS2HB16-Q1 , , TPS1HC100EVM , TPS1HC30EVM , TPS1HB08-Q1 Hi team,
Does it has TPS1HCxxx-Q1 series daughter card?
Do you have TPS2HB08…
Part Number: TPS1HA08-Q1 Hi Experts:
I'd like to know the condition which could trigger the auto - reverse protection in TPS1HA08-Q1, as the description in datasheet ,
"In the reverse battery condition, the switch will automatically be enabled (regardless…
Part Number: TPS1HA08-Q1 Hi team,
In our Design if the enable pin of TPS1HA08-Q1 is toggled (form High-Low-High and VIN = 12V) , we are observing the distortion in both Output and Input voltages and also Output Voltage reduced to 2V .
Please suggest the…
Part Number: TPS1HA08-Q1 Hi,
My customer has the following questions.
How long does it takes from detecting over current (exceeding current limit) to stopping output?
How long does it takes from detecting over temperature to stopping output?
Please…
Part Number: TPS1HA08-Q1 I am currently working with the TPS1HA08 chip and I believe i am having a fault error situation. Once the chip is enabled, it outputs the correct voltage and reads the appropriate current (both the power supply and SNS pin). However…
Part Number: TPS1HA08-Q1 Hello team,
I got the questions from the customer. Could you support those?
1: For Vbb(extended operating range), ds mentions "Device will function within extended operating range, however some parametric values might not apply…