Part Number: TPS1HB08-Q1 Tool/software: Hi Expert,
What is the maximum inrush current of the TPS1HB08-Q1?
Input Voltage 12V; TPS1HB08A-Q1, A version.
Thanks
Xiaoxiang
Part Number: TPS1HB08-Q1
Tool/software:
Hello All,
When operating at low VBB the RSNS value needs to be scaled to match this operating voltage. For an application reference, to get the correct ISNSFH values mentioned in the data sheet the following…
Part Number: TPS1HB08-Q1 Tool/software: Hi,
The SNS output is used to indicate system faults. ISNS will go to the predefined level, ISNSFH, when there is a fault.
According to SNS CHARACTERISTICS, when VBB = 6 V to 18 V, ISNSFH = 4mA to 5.3mA, typical…
Part Number: TPS1HB08-Q1 Tool/software: I wanna confirm the missing data in the datasheet
And I also want to know if they don’t use RLIM to limit current, Whether the current can exceed this value(104A) is as long as it does not exceed the junction…
Part Number: TPS1HB08-Q1 Tool/software: Hi team,
Could you share its thermal shutdown typ and max spec? Datasheet shows just "min" value as 150'C.
Regards, Ochi
Part Number: TPS1HB08-Q1 Tool/software: Hi team,
Customer found that the TPS1HB08FQPWPRQ1 is damaged when they did the power supply reverse test (Connect GND to 12V, Connect EXP_Pad to GND )
However, when the customer disconnect the MCU from the FLT…
Part Number: TPS1HB08-Q1 Tool/software: Hi Team,
Customer heard that some of the device has the tie-bar, while since the tie-bar is exposed outside, sometimes the rust may cause electron transfer and lead short issue. We would like to confirm that if…
Part Number: TPS1HB08-Q1 Tool/software: Hi team,
My customer is evaluating TPS1HB08-Q1 in their project and they have below questions. Could you please help give some comments?
The customer does not connect all Vout pin of TPS1HB08-Q1 together,…
Part Number: TPS1HB08-Q1 Tool/software: Hi,
I found, by chance, that the device (TPS1HB08AQPWPRQ1) does not become a FAULT state even if the current exceeds the ILIM, when EN is Low.
The scenario is as below.
1) EN is set HIGH to enable TPS1HB08AQPWPRQ1…
Part Number: TPS1HB08-Q1 Tool/software: Hi,
We are using TPS1HB08AQPWPRQ1 in the design. What is the reaction time to shutting down the HSS once current limit is reached?
Currently set value in design is 12A. I am getting current limit triggered …