Part Number: TPS1HTC30-Q1 Other Parts Discussed in Thread: TPS1HB08-Q1 Tool/software: Hi TI team,
I have some queries on TPS1HTC30-Q1 devices.
Q1. Can we connect TPS1HTC30-Q1 devices in cascading configuration? (continuous current of TPS1HTC30-Q1 is 6A…
Part Number: TPS1HB08-Q1 Hello team,
About the Thermal Considerations about HSS such as TPS1HB08-Q1, I only see the Rds(on) at max temp. But if we use HSS at 1kHz frequency, how can we calculate the switching loss of MOS when in thermal consideration?…
Part Number: TPS1HB08-Q1 Hi team,
Customer has a question about the current through SNS pin when the load is disconnected.
When the load is disconnected, does 1uA(max) of ISNSleak flow through SNS pin in the condition of VDIA_EN = 5V or 0V?
Regards,
S…
Part Number: TPS1HB08-Q1 Hi!
The datasheet for this IC says, that the user can connect the SNS-pin parallel to several TPS2HBXX, all SNS stay on Hi-Z remain until the one of them is selected. But, for example, the error occurs in the control microcontroller…
Part Number: TPS1HB08-Q1 Hi team,
Could you tell me which pocket quadrant shown in TAPE AND REEL INFORMATION is on TPS1HB08AQPWPRQ1 pin1?
Regards, Ochi
Part Number: TPS1HB08-Q1 Hi team,
Does TPS1HB08-Q1 have internal charge pump circuit?
How much switching frequency it is? When does charge pump operate or be disabled? (Ex. charge pump is enabled @ EN input voltage is H / it is disabled @ EN input is low…
Part Number: TPS1HB08-Q1 Hi all,
Could you explain detail about "some parametric values might not apply" ?
When or Which device works within "extended supply voltage" and "nominal supply voltage"
Which parametric values…