Part Number: TPS1HB35-Q1 Hi team,
Do we have any extended testing data or guidance for estimating min/max current values for a selected Rilim between 5kOhm and 25kOhm when doing a worst case analysis?
My current thought is to do a linear approximate…
Part Number: TPS1HB35-Q1 Hi team,
Do we have any extended testing data or guidance for estimating min/max current values for a selected Rilim between 5kOhm and 25kOhm when doing a worst case analysis?
My current thought is to do a linear approximate…
Part Number: TPS1HB35-Q1 Hi team,
Do we have any extended testing data or guidance for estimating min/max current values for a selected Rilim between 5kOhm and 25kOhm when doing a worst case analysis?
My current thought is to do a linear approximate…
Part Number: TPS1HB35-Q1 Hello,
I would like to understand better how to manage the component TPS1HB35(08)-Q1. TI classified this component as Functional Safety Capable, as per the table below:
So, if I understand well, this component is only QM…
Part Number: TPS1HB35-Q1 Other Parts Discussed in Thread: TPS1HB08-Q1 Dear Support Team,
We have used TPS1HB35-Q1 load switch in design, I would like to get your support to review the schematic.
Input = 14V
Output= 14V
Iout = 10.6A
Do we need…
Part Number: TPS1HB35-Q1 Other Parts Discussed in Thread: TPS1HB08-Q1 , Hello,
I would like to ask some Functional Safety questions on TPS1HB35(08)-Q1 component. I have the following safety manuals available:
- SafetyManual_TPS1HB08-Q1
- SafetyManual_TPS1HB35…
Part Number: TPS1HB35-Q1 Hi teams,
I want to use a High-side switch or load switch, the specification is similar to TPS1HB35-Q1, and then it needs EN pin/over-current and over-voltage protection,
but the input voltage is -6V, the output current is…
Part Number: TPS1HB35-Q1 Hi
The peak current is only 4A as below, but we have to set 30A current limitation by Ilim resistor, otherwise the output will be turned off as picture 2, schematic is also attached, could you please help? Thanks.
TI …
Part Number: TPS1HB35-Q1 Could you please tell details of Vtemp pin in transient Pspice model of the TPS1HB35A-Q1?
Is it for temperature analysis?
What should be its potential if we dont wish to do temp analysis?
Thanks and Regards,
Madhura…
Part Number: TPS1HB35-Q1 Hello,
I would like to switch on/off 24volt power to a load.
TPS1HB35-Q1seems a good choice. However nominal voltage is 18 volt although the datasheet says that it can work at up to 28 volt
7.3 Recommended Operating…