Part Number: TPS1HC100-Q1 Tool/software: I'm considering applying High-Side-Switch " TPS1HC100BQPWPRQ1".
I want to keep the DIAG_EN pin always High state (ON) by connecting it to +5V with a pull-up resistor without connecting it to the…
Part Number: TPS1HC100-Q1
Tool/software:
Dear Team, do we have figure 6-9 of the datasheet with different resistor values? Required values:
39k
47k
56k
If not, could you please help to give an estimate on how to calculate it and what to consider?
…
Part Number: TPS1H100-Q1 Other Parts Discussed in Thread: TPS1HC100-Q1 , , TPS25948
Tool/software:
Please note that I got the part number confused in the title, I am inquiring about TPS1H100-Q1 and not TPS1HC100-Q1. The reason being that only TPS1H100-Q1…
Part Number: TPS1HC100-Q1 Other Parts Discussed in Thread: TPS1HC30-Q1 Tool/software: Hello, Team,
We have a question from our customer when using two TPS1HC100-Q1 which are configured to not turn on at the same time.
Can those two HSS share the same…
Part Number: TPS1HC100-Q1 Our customer is considering to use TPS1HC100BQPWPRQ1.
They have some questions.
1.About the current sense (detection) function To enable the current sense function, should I input "Hi" to the DIAG_EN terminal? Is it correct…
Part Number: TPS1HC100-Q1 Hi,
1) Could you explain how to simulate Thermal shutdown behaviour using Tj and Tcon in Psipce simulation? Can u share any example?
2) In data sheet section 8.1, it is mentioned that " The current-sensing function operates normally…
Part Number: TPS1HC100-Q1 1) Could you explain "swing detection" which is mentioned in the features section. Is it "ringing effect" ?
2) Could you share Minimum & maximum hysteresis voltage on EN pin (VIHYS, EN)?
3) Could you please…
Part Number: TPS1HC100-Q1 Other Parts Discussed in Thread: TPS1HC30-Q1 , 1) Should we use ILIM resistance only between 7.15kΩ to 71.5kΩ ? Can I use 5.1k as R_ILIM to limit current of 7A? (If yes, what is the KCL value i should consider as it not mentioned…
Part Number: TPS1HC100-Q1 Other Parts Discussed in Thread: TPS1H100-Q1 1: Is there a problem with the 1.8V IO input voltage?
2: Is the diagnosis of ST output a change in high and low IO
3: Current value RCL=1.23 * 2000/Iout. If calculated using 2.2K, Iout…