Part Number: TPS1HC100-Q1 I’m using this component new into my design: TPS1HC100BQPWPRQ1
Previously I was using TPS1H100AQPWPRQ1 which EN pin Vin High was 2V
That’s why Im using a digital switch to provide 3.3V to EN pin. Using 1.8V from SoC to…
Part Number: TPS1HC100-Q1 Hi team,
My customer is using TPS1HC100 and want to test it for short protection. When they short OUT to ground, the device seems not working normally on the fault pin value.
Yellow channel is for Fault pin, pink channel is…
Part Number: TPS1HC100-Q1 Other Parts Discussed in Thread: TPS22950-Q1
This switch is for a usb hub TUSB4041-Q1
Please review the schematics, this switch is not working.
Part Number: TPS1HC100-Q1 Other Parts Discussed in Thread: TPS1HC30-Q1 , TPS272C45 Hello,
I am using a high-side driver (TPS1HC100-Q1) to drive an inductive load.
The single pulse turn-off energy for this high side driver is 35mJ.
But, energy stored in…
Part Number: TPS1HC100-Q1 Hi team,
One of VBB (for example, pin-12) is opened but another one (for example, pin-13) is connected, what happen?
One of VOUT (for example, pin-9) is opened but another one (for example, pin-10) is connected, what happen?
…
Part Number: TPS1HC100-Q1 Other Parts Discussed in Thread: TPS1HB08-Q1 Hello,
I am looking for ‘ Single Pulse Inductive Load Switching Energy‘ for two TI high side driver ICs:
1) TPS1HC100-Q1
2) TPS1HB08-Q1
Request you for the info.
kind regards…
Part Number: TPS1HC100-Q1 Hi Team,
Figure 8-3 of this devices datasheet shows a current source if I OUT / K ILIM being sourced out of the ILIM pin.
Can someone confirm that K ILIM = K CL ? K ILIM doesn't seem to appear anywhere else in the datasheet.
Thanks…
Part Number: TPS1HC100-Q1 Other Parts Discussed in Thread: TPS27SA08 , TPS1HC30-Q1 I have to run a heater at 12V 10A 120W or 24V 5A 120W . Can TPS1HC100BQPWPRQ1 handle these requirements? These are the maximum values that i am expecting. In practical, it…
Part Number: TPS1HC100-Q1 Hello Team,
Currenly we are using TPS1HC100-Q1 as a high side stage . This is used for contactor control . We also have a low side which is pwm control. Using this High side we only turn on or off the high side. Currently i read…
Part Number: TPS1HC100-Q1 Hi Team,
I pulled down and am working with the TPS1HC100B-Q1 PSPICE model from the TI website.
Can someone explain what the “TJ” and “TCON” pins are on the PSPICE model, as these are not actual pins on the device? My assumption…