Part Number: TPS1HC100-Q1 Hello Team,
Currenly we are using TPS1HC100-Q1 as a high side stage . This is used for contactor control . We also have a low side which is pwm control. Using this High side we only turn on or off the high side. Currently i read…
Part Number: TPS1HC100-Q1 Hi Team,
Figure 8-3 of this devices datasheet shows a current source if I OUT / K ILIM being sourced out of the ILIM pin.
Can someone confirm that K ILIM = K CL ? K ILIM doesn't seem to appear anywhere else in the datasheet.
Thanks…
Part Number: TPS1HC100-Q1 Other Parts Discussed in Thread: TPS27SA08 , TPS1HC30-Q1 I have to run a heater at 12V 10A 120W or 24V 5A 120W . Can TPS1HC100BQPWPRQ1 handle these requirements? These are the maximum values that i am expecting. In practical, it…
Part Number: TPS1HC100-Q1 Hi Team,
Can you please clarify the inquiry below?
Can we use TPS1HC100-Q1 for driving inductive load with a switching frequency of around 40hz to 100hz. Also one more query i am driving an inductive load of around 16 mH with a…
Part Number: TPS1HC100-Q1 Hi Team,
I pulled down and am working with the TPS1HC100B-Q1 PSPICE model from the TI website.
Can someone explain what the “TJ” and “TCON” pins are on the PSPICE model, as these are not actual pins on the device? My assumption…
Part Number: TPS1HC100-Q1
Hi Expert,
I have several questions about TPS1HC100-Q1:
1. As you can see below, the relative shift down has tighter threshold than absolute thermal shut down. So relative one always happens first. So under what condition d…
Part Number: TPS1HC100-Q1 Hi Team,
Customer question below:
It seems the TPS1HC100 and other similar high-side switches have a maximum PWM frequency of 2 kHz. Does TI have a smart high side switch that has a higher PWM frequency? ( could be up to 20 kHz…
Part Number: TPS1HC100-Q1 Hi Team,
Can you please clarify if there are any internal pull up on the fault pin of PTPS1HC100BQPWPRQ1?'
is this internal pull up for output open load or internal pullup on the fault pin ?
Thank you in advance.
Regards…
Part Number: TPS1HC100-Q1 Hello, Team,
We have a question about TPS1HC100-Q1 when DIAG_EN is unused (open or connected to GND via R PROT resistor.)
Datasheet p30 states that:
however, DIAG_EN being high is not necessary for all protection features to…