Part Number: TPS2001D Hello,
Our customer has asked if TPS2001D is damaged at EN=Low with/without certain power supply.
case-1 : VIN=off (0V), EN=off (Low : disenable), VOUT=5.5V
case-2 : VIN=on (e.g. 5V), EN=off (Low : disenable), VOUT=5.5V.
I suppose…
Part Number: TPS2001D Other Parts Discussed in Thread: TPS2069 , TPS2061 , TPS2051 , TPS2041
Hi
TPS2001D is promoted to be 2nd source of RT9742CGJ5F, which is Flip chip, however, this package thermal resistance is 126.5C/W, very lower than 220 C/W of TPS2001D…
Part Number: TPS2001D Other Parts Discussed in Thread: TPS2065D , hi,
My customer asks for the IEC 62368-1 ed3.0 test report for TPS2001D and TPS2065D.
can you provide it?
I only can find the certification for TPS2001D and TPS2065D.
US-34988-UL Certificate…
Part Number: TPS2001D Hi team,
My customer is looking for USB power switch and they have concerned about the vin voltage range of our TPS2001d.
From the datasheet, it shows the vin range from 4.5v to 5.5v. They would like to know what will happened if…
Part Number: TPS2001D Other Parts Discussed in Thread: TPS2001C , Hi support team,
What is the difference between TPS2001D and TPS2001C?
Is there anything other than the following? TPS2001D is lower cost than TPS2001C. TPS2001D does not have a package equipped…
Part Number: TPS2001D According to the thermal equations of TPS2001D datasheet in DBV package:
Pd=2*2*0.09=0.36W Tj=60°C+0.36*220.4=139°C
Questions:
1) Can we review the junction temperature 139°C based on above condition? How to reduce Junction…
Part Number: TPS2001D Hi Team,
Can you please confirm that TPS2001D can B2B to replace SY6288C20AAC (2A/ active high)?
https://datasheet.lcsc.com/szlcsc/Silergy-Corp-SY6288C3AAC_C207612.pdf
BR,
SHH
Part Number: TPS2001D Hi Sir,
My customer recently encountered a problem with TPS2001D. After doing pulse output short test, it get burned and damaged.
May refer to the waveform below. The output peak current is up to 60A while the limited current…
Part Number: TPS2001D Hi Team,
Could you please let me know if FLT pin can be tied to GND in case that this pin is not used? Looking at the datasheet, it is open-drain output and looks no problem.
Regards, Nobuhiko Wasa