Part Number: TPS2051B Other Parts Discussed in Thread: LM74700-Q1 , TPS2051 , TPS2553 I need the following protection for a simple 5V input circuit 1: Over voltage 2: Over current 3: Short circuit 4: reverse polarity 5: reverse current It clearly not meeting…
Part Number: TPS2051 Other Parts Discussed in Thread: TPS2514 , Hi Sir!
I wanna make a usb host device (android , ios / smart device usb power).
I need to 5V / 0.5A usb max power like a PC usb port.
I'm think about TPS2514 and TPS2051.
is it possible…
Part Number: AM3358 Other Parts Discussed in Thread: TPS2051 , TPS2041B , TPS2051B
Hi,
AM3358, TPS2051BDGN and TPS2041BDGN.
Kernel 5.11.10
I have a custom board based upon the BBB. USB0 is in HOST mode and will supply +5vdc using the TPS2051BDGN power…
Other Parts Discussed in Thread: TPS2051 Hi all,
Some customers here plan to remove TPS2051 to save the cost and require the USB only work in host mode, so how to modify the dts file of the AM335x kernel to support it?
Thanks!
Part Number: TPS2051B Other Parts Discussed in Thread: TPS2051 , Hello
I saw TPS2051 TI document sheet-23 figure-39 for about inrush current with different load capacitance as the file attached.
Could you advise me what maximum spec of capacitance? And…
Other Parts Discussed in Thread: MAX3232 , XTR111 , ISO7421 , TPS2051 , TPD4S012 , LM4040 Dear Sir / Madam,
Please find below TI IC part number which is used in our project.
MAX3232/SOIC-Thin
XTR111(MSOP-10)
CD74HC147M
ISO1050DUBR
ISO7421
TPS2051…
Hi Miranda,
Please check TPS2041, TPS2051, TPS2061 and TPS2065, TPS2069
For TI's policy, I will first click resolved button.
If you have any other concern, contact me any time.
If you think resolved, please help click 'Issue is solved button'.…
Hi Liu,
What do you mean repairing #1 and #2? Replace it and change a new IC? And then damaged?
1. To power VIN of TPS2051 with a separate DC supply instead of buck and power cycle to check whether have same issue.
2. Power the IC with the original configuration…