Part Number: TPS2061C Hi There,
We have situation on design, where we had left the EN_n PIN of the Device Un-Connected.
We want to know whether there is any PULL-DOWN on the Enable Pin in the device to have the Load Switch always enabled condition.
Thanks…
UPDATE: the part we are currently using IS TPS2061CDBVT . A few months back I got an older datasheet from DigiKey web site - they have fixed this. So, I am ALREADY using the part you suggested. Apologies for the confusion...
Now I'm confused. Why did PC power…
Part Number: TPS2064C Other Parts Discussed in Thread: TPS2561 , TPS2003C Dear team,
Could you send me the CB report of TPS2061C ? I need IEC62368-1 or EN62368-1 CB.
Best Regards, Watanabe
Part Number: LMZM23600 Other Parts Discussed in Thread: TPS2061C Hi,
I am considering using the LMZM23600 to supply power for our host USB port, but I want to sanity check this.
As I understand it the LMZM23600 can
Switch 24V to 5V (we have a 24V system…
I think I know why \FLT is asserted when \EN is high on the TPS259573. The \EN pin is actually an OVLO input on this device, so turning off the output by taking \EN high flags an OVLO fault. The TPS259533 also does the same thing, which I did not expect…
Hi Detlef,
So it appears the application is similar to a 1-cell power bank?
We have some documentation here:
http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=slpt027&fileType=pdf&keyMatch=powerbank&tisearch=Search-EN…
Other Parts Discussed in Thread: TPS2041B , TPS2061C , TPS2068C Hello all,
This is my first post to the forums so don't beat me up too bad. :) I was wondering what the scope plot of a 2041B "should" look like. We currently are hitting our circuit…
Part Number: TPS2065C Other Parts Discussed in Thread: TPS2069C , TPS2051 Dear expert,
Basically i want to power on the BBB with 5V 2.5A
because i need 1.5A power on USB port
hence i decided to make custom BBB it will exactly same as current BBB with a…