Part Number: TPS2062 hi Team,
OEMs wants to project the voltage input to the battery pack.
the abs max voltage for the pack+ pin is 30V, they concern that externally might have 48V from the adaptor if the front end malfunction
the maximum current that…
Part Number: TPS2062 Please send it after filling out the specification comparison table for our mass-produced products and the two materials that are in stock at ti.com below.
M3201-000632
TI.COM
TI.COM
TPS2062QDGNRQ1
TPS2062DGA4
…
Part Number: TPS2062 The datasheet says the input is TTL and CMOS compatible, but does not mention if there is an internal pulldown or pullup. Can it be left unconnected?
Part Number: TPS2062 Hi,
This is David from Bureau Veritas Taiwan, the third-party testing laboratory in Taiwan. We're dealing with a multimedia product to get it tested in terms of Taiwan regulations. TPS2062DGN is used in the device and we need IEC…
Part Number: TPS2061 Other Parts Discussed in Thread: TPS2051B , , TPS2066 , TPS2062 , TPS2065 Tool/software: Hi team, The datasheet has been changed ( revJ -> K ) and Overcurrent trip threshold has been removed. Why is this? BR, Kengo.
Part Number: TPS2062C Other Parts Discussed in Thread: TPS2062 Hi Team,
Could you tell me the differences between TPS2062 and TPS2062C?
Regards,
Takashi Onawa
Part Number: TPS2062 we need for the certification of our devices that the IC "TPS2062" complies with the test specified in the standard according to IEC 60950-1, Appendix CC (or UL 60950-1, Appendix CC) for USB interfaces. Is the module certified…
Part Number: TPS2062 Hello,
I have a couple of quick questions in regard to TPS2062 device. I'm using only one channel of this device to power a USB 3.0 connector. This device will be located on the I/O board close to the USB 3.0 connector in a SFF chassis…