Part Number: TPS2066 Other Parts Discussed in Thread: TPS2553 Tool/software: Hello,
We are using TPS2066D to control VCC supply to USB 2.0 connector which connects to bus-powered or self-powered USB devices. The intention is to supply 5v on USB VCC…
Part Number: TPS2066 Hi Team,
I'm planning to the use the power switch TPS2066DGNR for controlling the 5V VBUS to the USB 3.0 connectors. As the each USB 3.0 power requires 0.9A current, and TPS2066DGNR is capable of providing output of 1A per channel…
Part Number: TPS2066 Greetings from iWave Systems Technologies Pvt. Ltd.
We are evaluating the below Texas Instruments components for use in one of our medical products.
Part Numbers:
TPS2066DGNR
TPS3808G33DBVR
TPS386000RGPR
TPS4H000AQPWPRQ1…
Part Number: TPS2066 Tool/software: Hi
Could you help provide the TPS2066DR UL & CB certificates
Also, what is the difference between TPS2066DR and TPS2066C?
Thanks
Part Number: TPS2066-1 Hi, Team,
Does TPS2066DGNR-1 have IEC62368-1 3rd certification? If yes, could you send me the report?
Best Regards, Satoshi Yone
Part Number: TPS2066 Hello Expert,
I have some question and request.
1. Are all TPS206x Sereis CB Certificated? or Is TPS2066 CB Certificated?
2. Could you send CB Certified Report to me by e-mail?
michael.jeong@arrow.com
Best regards…
Part Number: TPS2066 HI team,
We want to check if we only use one channel of TPS2066, the device can support 1A. If we use two channels TPS2066, the device can support 2*1A or 2*0.5A? Thanks.
Part Number: TPS2066 If I only use 1 channel of TPS2066CDR, how to connect pin OUT2, FLT2, and EN2?
Is is ok to connect like below?
EN2 - GND
OUT2 - NC
FLT2 - NC
Best regards,
Yuta
Hi Zhang,
small difference - big change!
You are perfectly right. We looked into the data sheets and also bought some TPS2066 - now they work fine.
Thank you for your assistance!
Best regards
Ulf
Part Number: TPS2066 What happens if OUT1 or OUT2 is driven externally by mistake and the driving voltage is higher than the input voltage, will it back drive the IN pin?