Part Number: TPS2066-1 Hi, Team,
Does TPS2066DGNR-1 have IEC62368-1 3rd certification? If yes, could you send me the report?
Best Regards, Satoshi Yone
Part Number: TPS2066 Hello Expert,
I have some question and request.
1. Are all TPS206x Sereis CB Certificated? or Is TPS2066 CB Certificated?
2. Could you send CB Certified Report to me by e-mail?
michael.jeong@arrow.com
Best regards,
Michael
Part Number: TPS2066 HI team,
We want to check if we only use one channel of TPS2066, the device can support 1A. If we use two channels TPS2066, the device can support 2*1A or 2*0.5A? Thanks.
Part Number: TPS2066 If I only use 1 channel of TPS2066CDR, how to connect pin OUT2, FLT2, and EN2?
Is is ok to connect like below?
EN2 - GND
OUT2 - NC
FLT2 - NC
Best regards,
Yuta
Part Number: TPS2066 Folks,
coming back to the TPS2066 Enable Pins:
We want to use the device as a simple Undervoltage Protection Switch. Our external supply is a One Cell LiIon battery, which works properly in a range of 3.0 to 4.2 Volts. This source…
Part Number: TPS2061 Other Parts Discussed in Thread: TPS2051B , , TPS2066 , TPS2062 , TPS2065 Tool/software: Hi team, The datasheet has been changed ( revJ -> K ) and Overcurrent trip threshold has been removed. Why is this? BR, Kengo.
Part Number: TPS2066 What happens if OUT1 or OUT2 is driven externally by mistake and the driving voltage is higher than the input voltage, will it back drive the IN pin?
Part Number: TPS2066 Other Parts Discussed in Thread: TPS2553 The TPS2066 allows reverse current to flow in the case where EN is held high (switch enabled) and the OUT pin is at a higher voltage than the IN pin. See the link below:
https://e2e.ti.com/support…