Part Number: TPS2113A
Hi~
IN1=MAIN POWER(OFF STATE, 0V), IN2=BATT connected.
As shown in the picture, EN=LOW and VSNS=52ms high were applied.
VOUT does not become IN1(0V) even during VSNS=HIGH(52ms) and IN2(BATT) is output.
It is confirmed that the output…
Part Number: TPS2113A Hi~
In the 2113A 7-page truth table, what is the output if enable is always low(0) and Vsns is floating (not connected)?
Best Regards.
Part Number: TPS2113A Hi,
Good Day.
The customer is looking for Power Path Controller/Switcher that can switch between three sources.
He saw a few eFuses, those in the Oring application would be an alternative but mainly it's around 300W switching between…
Part Number: TPS2113A Other Parts Discussed in Thread: TPS2121 Dear Sir or Madam,
my question regards to set two TPS2113A in parallel to get a higher current delivery. Unfortunately I cannot find an alternative switch with the same conditions but with…
Part Number: TPS2113A Other Parts Discussed in Thread: TPS2116 If I have a TPS2113A device with these initial conditions: #EN=0V, VIN1=0V, and VIN2=0V, and then I switch on a 3V input to VIN1... what is the rise time on the output as it goes from 0 to…
Part Number: TPS2113A Hi,
I am working on some derating activity for this device, but i am not able to find all the information i need from the datasheet.
I see there is the rdsOIN curve in figure 8 of the datasheet, but do you have one for the max rds…
Part Number: TPS2113A Other Parts Discussed in Thread: TPS2116 , TPS2121 I have the following schematic in my design.
XFMR_OUT (IN2) is always on. HSEC_5V0 (IN1) is turned on and off.
When I turn HSEC_5V0 (IN1) on, sometimes the output of the switch starts…
Part Number: TPS2113A Other Parts Discussed in Thread: TPS2113 Hi,
We are looking to use TPS2113 to Mux two 5V supplies. One from a 5V regulator 2A and one from 5VUSB. I tried to design the circuit such that, IN1 (5V external) is prioritized and switches…