Part Number: TPS2113A Hi team,
My customer is using the TPS2113A now, when remove VBAT_DC_5V, 5V_Cap will sink the current to IN1, we want to check whether the phenomenon is right or not. Thanks
Part Number: TPS2113A Support Path: /Product/Production, ordering, and quality/ Hi,
We are using the TI part TPS2113ADRBT but we couldn’t get the material declaration on the website (it’s unavailable for this part).
I have also tried the pull…
Part Number: TPS2113A Other Parts Discussed in Thread: TPS2113 When Vin1(V_5V_S) goes power down, there is a rining on OUT(V_BAT_4V) of TPS2113.
Is that the normal in TPS2113.
Customer is looking for a solution for voltage switch OUT=IN1/IN2 bease on the…
Part Number: TPS2113A Other Parts Discussed in Thread: TPS2115A , TPS2115 Hi TI,
I have a few questions about the TPS2113A and the TPS2115A.
My product requires me to switch between a local supply and a backup supply to keep an IC powered. Both rails are…
Part Number: TPS2113A Other Parts Discussed in Thread: TPS2113
Hi,
my customer is using the attached circuit where he put 2 diodes in parallel to the device , just to increase current capabilities during peaks.
They noticed that with the diodes the…
Part Number: TPS2113A Hi.
I have a question regarding the TPS2113A. How does one define the threshold voltage when the TPS2113A will automatically switch from IN1 to IN2? Is there a formula like voltage divider since I could not understand it from the…
Hi Team,
I would like to know about jumpers setting of “mode1 automatic switching”.
If jumper3 and 4 is open, VSNS pin is open.
Is this setting correct?
I understand that VSNS pin have to connect GND because VSNS pin is the input of comparator…
Hi Team,
We are evaluating TPS2113AEVM at the mode1 automatic switching.
Are Q1 and Q2 of this device turned off at the same time if when IN1 and IN2 became the same voltage?
[Background]
We are evaluating TPS2113AEVM at the following condition.
Then…
Other Parts Discussed in Thread: TPS2113A Hi Team,
Our customer would like to use TPS2113A in AUTO-SWITCHING MODE.
I understand that the switch of this device is selected to the higher input voltage if an input voltage difference(IN2-IN1) is more…
Other Parts Discussed in Thread: TPS2113A Hello Team,
Could you tell me the minimum rating of current limit accuracy for TPS2113A at RILIM = 250 Ω?
Customer would like to know the proper rating of current limit if output current is 1.4A.
Best Regards…