Other Parts Discussed in Thread: TPS2113A I am testing out the TPS2113A device on a breadboard. The current limit is set to 1A (Rilim=500R). The OUT pin is connected to an electronic load (set as a 900mA constant current load), IN1 is supplied from a programmable…
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: TPS2113A , TPS2115A Hi,
Greetings!
I would need to simulate TPS2115ADRBR using PSpice for TI in order to know the I/O operations for our system.
Unfortunately, I was not able to find any .cir / …
Hi Shibin,
Neither the TPS2113A nor TPS2115A can support 2A of current. Both the TPS2113A and TPS2115A devices are only rated for 1.25A.
Is 2A of current to the output needed for your application?
If 1.25A is acceptable, I would recommend the TPS2113A…
Other Parts Discussed in Thread: TPS2113A , TPS63001
Hello,
I'm having some trouble with a tps2113a. I've connected it as shown in Figure 14 in the datasheet.
IN2 is not connected at the moment, but IN1 is connected to 4.9V.
With my setup the switch…
Part Number: LM66100 Other Parts Discussed in Thread: TPS2113A , TPS2110A , TPS2111A , TPS2114A , TPS2115A , TPS2112A , TPS2116 Hi, I have a related question to this topic. We know that it's generally not a good idea to put batteries in parallel because one…
Other Parts Discussed in Thread: TPS2113A We have a customer trying to implement the logic bounded by the red dashed line in the attached schematic. The TPS2113A would work well in this application, but it is too expensive. The customer would like a solution…
Part Number: TPS2115A Other Parts Discussed in Thread: LM66100 , , TPS2113A , TPS2115 , TPS2113 , TPS2116 Hi, Our current application design requires two similar sets of 4.2V batteries as primary and secondary power sources. Previously, we were first considering…
Part Number: TPS2116 Other Parts Discussed in Thread: TPS2115 , TPS2113A , TPS2113 , Hi all, I am considering using two TPS2116 in series to create a switching mechanism between 3 power supplies. I want to switch between a barrel jack, USB and a off board header…
Part Number: LM76003-Q1 Other Parts Discussed in Thread: TPS2113A , TPS61022 , LM76003 , TPS2113 , Hi sir,
We measure the abnormal waveform on VSYS_3V8, which is power mux (TPS2113A) output.
Test method:
Provide DLC_IN with 12V, LM76003Q output 4V.
Provide…
Hi Ramon,
Your new setup looks to be automatic switchover and not manual switchover. This will work but it is not ideal as there is a wide voltage window between high and low on the Dx pins.
The TPS211xA PowerMUXes are a family and we actually have a…