Part Number: TPS2115A Other Parts Discussed in Thread: TPS2115 , TPS2116
Hello Expert,
May i know the main different between TPS2115PW VS TPS2115APW ? both are TSSOP-8 (PW) package.
we are selecting between them, but i can tell the different from datasheet…
Part Number: TPS2115 Hello,
I am interested in using TPS2115 for a design but I am not sure if it is suitable for both manual/autoswitching. Would it be possible to have both mecanisms with this device? I wonder if I can control the switch between supplies…
Part Number: TPS2115 Other Parts Discussed in Thread: TPS2116
Hi All,
I have a question about TPS2115.
With IN1 (8pin) open, 5V was input to IN2 (6pin) and D0 (2pin). I checked the voltage with IN1. What is the cause of this?
Best Regards, Ishiwata
Part Number: TPS2115 Other Parts Discussed in Thread: TPS2113A , , TPS2116 Hello!!
I am having trobles with the Hysteresis in this circuit.
A ripple in the inputs makes the output switch permanet the inputs.
I am thinking of adding an external comparator…
Part Number: TPS2115 Hi Team,
We are using TPS2115ADRBR part in our design where we are connecting two different inputs as shown in the below image.
In the design we have pulled D1 to GND and used a DIP switch to D0 . So whenever the D0 pin is LOW , irrespective…
Part Number: TPS2115 Other Parts Discussed in Thread: TPS2121 , TPS2120 , TPS2113 Hello, here is my setup:
-I use TPS 2115 in autoswitching mode
-Two Li-Po batteries are connected at inputs In1 and In2.
-Load current is 0.8A (constant power).
Problem is that…
Part Number: TPS2115 Other Parts Discussed in Thread: TPS2120 , TPS2121 , Hi.
I am planning to use TPS2115 for powering device from USB with additional external power supply as option. But I need to transfer more than 1.25A that can be handle by TPS2115…
Part Number: TPS2115 Hi,
I want to design an auto switch configuration from two power supplies of 5V@3A.
What should be the inputs D0 and D1 in order to do so, it's not straightforward from the datasheet because in figure 14. the D0 is floating and D1…