Part Number: TPS2116 Hello,
i would like to use TPS2116 for uSD card voltage transition 3.3V -> 1.8V; i have a few question regarding power sequencing on TPS pins.
I need to work with MODE manual for manually controlling Piority (SD_VSEL); in my design…
Part Number: TPS2116 I am trying to simulate the TPS2116 in Tina TI before I use it in a design.
In my actual use case, Vin1 will be tied to 5 V from a USB connector, and if that is not present I want it to supply the power from Vin2 instead, thus I…
Part Number: TPS2116 Hello,
We are using the TPS2116 in the priority configuration where VIN1 is driven by a 4V5 source and VIN2 is a backup driven by a battery at a voltage between 3V3 and 4V2.
We are testing a prototype and have observed that during…
Part Number: TPS2116 Hi Team,
Good day!
We are facing an issue with the TPS2116. When the secondary voltage is applied to IN2, the device is consuming around 220 µA.
We kindly request your support in resolving this issue.
The device is working…
Part Number: TPS2116 Hello,
Regarding the PR1 voltage reference on TPS2116DRLR, is there a characteristic curve that shows its behaviour over temperature?
Regards
Martin
Part Number: TPS2116 Hi,
I haven't found this specific information. Is the TPS2116DRLR.A obsolete? I don't see it mentioned on the datasheet, advertised on TI's website, or in Accuris. Also the website has a banner stating if we order the TPS2116DRLR…
Part Number: TPS2116 Hi Madam/Sir,
I have one question regarding TPS2116 power switch MUX. I'm looking to clarify my understanding of the documentation about the truth table (section 7.3.1 in d/s). I have a very simple circuit with two input power supplies…
Part Number: TPS2116 Tool/software: Hi Team,
my customer is now evaluating TPS2116 as following, could you please check whether it is good to use? Thanks.
VIN1 and VIN2 are two different inputs, could we use a MOSFET(control by GPIO) to bypass…
Part Number: TPS2116 Hello TI Team,
I am using the TPS2116 as a dual-input power multiplexer between USB 5 V (VIN1) and a regulated 5 V battery rail (VIN2) for a flight controller design.
I would like clarification on the following points:
1.…