Part Number: TPS22810-Q1 Tool/software: Hi team,
I only see the IMAX value for above 65 degree. What is the IMAX for -40-65 degree? Do we have a curve to implement this?
BR,
Bengi
Part Number: TPS22810-Q1 Tool/software: Hello,
I would like to have some help with the Failure Mode Distribution for the following part number TPS22810TDBVRQ1, this is usually included in the Functional Safety FIT Rate, FMD and Pin FMA report, but I cannot…
Part Number: TPS22810-Q1 Other Parts Discussed in Thread: TPS22810 , TPS1H000-Q1 , TPS4H160-Q1 , TPS22919-Q1 Tool/software: Can the Vin of TPS22810 be directly connected to car battery? We had issues before where devices rated 18v were damaged when directly…
Part Number: TPS22810-Q1 Hi,
I'm currently using the TPS22810TDBVRQ1 for switching the power supply of a battery operated device, but I need to provide up to 3.5-4 Amps at times. the TPS22810TDBVRQ1 Imax is 2A so i need a replacement with very low Iq…
Part Number: TPS22810-Q1 Hi team,
Could you advise if this device survives at the following condition?
VIN=0V unpowered.
VOUT = 12V (VBAT peak <18V)
Absolute maximum ratings of OUT pin is rated for VIN max, so I wonder if OUT pin can be survived if…
Part Number: TPS22810-Q1 Hi Team,
We are using the TPS22810TDBVRQ1 switch to control the 3.3V power supply. However, we have encountered a problem where there is a back drive from the VOUT pin to the VIN pin of the IC when the switch is not enabled. Is…
Part Number: TPS22810-Q1 Hello support team,
Would it be possible to use the quick output discharge pin if VOUT is not being used? I just want to use the quick discharge functionality that this part offers without actually using it as a load switch. …
Part Number: TPS22810-Q1 The data sheet of the TPS22810-Q1 contains a table with different values for the CT cap.
In the table there are also rise times for CT = 0 F
Also at different positions in the data sheet there is either the CT completely ommited…