Part Number: TPS22811 Tool/software: I am using TPS22811 in our design for 12V application. We have around 500uF capacitance on the output of TPS22811. If I just pull high the EN_OVLO pin for power cycling the IC is not turning ON again.
I cannot see any…
Part Number: TPS22811 Other Parts Discussed in Thread: TPS2811 Tool/software: dears,
could TPS2811 limit the output current after start-up?
i could not understand the note in the datasheet " The current limit circuit employs a foldback mechanism.…
Hi Chase,
Can we have a quick meeting regarding this. I think I am little confused here. My understanding till now is they have connected POE converted to 12V at the input of load switch and 12V DC adaptor at output of load switch. Not sure where the…
Part Number: TPS22811 Other Parts Discussed in Thread: SN74AHC1G02 Tool/software: Could you help me to review the schematic of TPS22811?
I use the output pin of SN74AHC1G02 as TPS22811's enable pin. The output signal NOR_5V_OUTPUT is 5V.
Part Number: TPS22811 Tool/software: Below is the overall on how the components are connected.
Please ignore the similarity in the net names because they are not part of the same project files. However, they are connected physically via cables.
Refer…
Part Number: TPS22811 Tool/software: https://www.ti.com/lit/ds/symlink/tps22811.pdf
The datasheet for the TPS22811 lists Pin10 as DNC = "Do not connect anything to this pin".
Is this just a strange wording for No-Connect, or would something…
Part Number: TPS22811 Tool/software: I was wondering if I could use this load switch at 10A? Would this destroy the device or reduce its useful life?
Thanks