Part Number: TPS22811 Tool/software: Dears'
The TPS22811 has a Quick Output Discharge (QOD) function, but the time it takes to discharge using this function is still slow on my system.
Is there any way to improve the circuit to discharge the Voltage…
Part Number: TPS22811
Tool/software:
Dear TI experts,
My customer considers TPS22811 for specific purpose.
They chek the step as follows, based on block diaram of TPS22811.
1. Apply 12V to output, and leave input floating.
2. FFT signal is…
Part Number: TPS22811 Other Parts Discussed in Thread: SN74AHC1G02 Tool/software: Could you help me to review the schematic of TPS22811?
I use the output pin of SN74AHC1G02 as TPS22811's enable pin. The output signal NOR_5V_OUTPUT is 5V.
Part Number: TPS22811 Other Parts Discussed in Thread: TPS61288 Hi support team, I am thinking of connecting TPS22811 after TPS61288 as shown in the figure below.
TPS22811_square_wave.pdf
Input 12V, 4.15A. Input 0.1515s pulse to EN. At this time,…
Part Number: TPS22811 Tool/software: I was wondering if I could use this load switch at 10A? Would this destroy the device or reduce its useful life?
Thanks
Part Number: TPS22811 Tool/software: https://www.ti.com/lit/ds/symlink/tps22811.pdf
The datasheet for the TPS22811 lists Pin10 as DNC = "Do not connect anything to this pin".
Is this just a strange wording for No-Connect, or would something actually…
Part Number: TPS22811 Other Parts Discussed in Thread: TPS2811 Tool/software: dears,
could TPS2811 limit the output current after start-up?
i could not understand the note in the datasheet " The current limit circuit employs a foldback mechanism.…
Part Number: TPS22811 Hello,
The analog current sense output on the IMON pin is proportional to the current through the FET. How does this behave when the current is flowing from the device OUT to IN (either through the FET body diode or from source…