Part Number: TPS22811
Hi,
I am implementing TPS22811LRPWR in a hot swap design.
When the device is not connected to the backplane the PRESENT# signal is floating and when the device is inserted the PRESENT# signal is pulled to GND. This is the…
Other Parts Discussed in Thread: TPS22811 Dear,
I am trying to simulate a circuit containing the TPS22811 IC with PSpice for Ti. Looking at the TI website , there should be a transient pspice model of that IC. However, I am unable to find that model…
Part Number: TPS22811 Hi
Please suggest suitable products When the dc-dc is transferred out to 3.3V, it will be connected to an external device, and it needs to be protected against external overcurrent, current limit 2.5A
Part Number: TPS22811 Hi TI support,
I am reaching out as I am trying to use the TPS22811EVM evaluation board for testing, but the output is not providing the expected voltage.
Our setup is as follows:
12V in on the power input
An adjustable DC…
Part Number: TPS22811 Other Parts Discussed in Thread: TPS25981 Imon pin in this chip can be used as setting current limit?
How can I calculate it, if my device the max current limit is 600mA, and could you share me the circuit fig.
In this EVM board…
Part Number: TPS22811 Hi all.
I want to turn on/off the power to a servo. The datasheet only talks about resistor dividers on the EN and /EN pins.
What is the proper way to turn the powerswitch on and off from a microcontroller pin? And do I still…
Part Number: TPS22811
Hello all,
This is my design for the issue described below:
I have a problem when I try to reduce voltage after the switch is off due to OVP
1. I'm powering up the switch at UVP state (4V) and the switch is off as expected…
Part Number: TPS22811 Other Parts Discussed in Thread: TPS25981 , TPS25946 , TPS2597 Hi team,
Can you tell me how much output voltage drop occurs when operating in the following order? I would like to know if there is any way to simulate this. Case…