Part Number: TPS22860 Tool/software: Hi,
Would like to check on the following
1. Recommended pull down resistor to the ON pin if driven by a tristate driver.
2. How will the pull down resistor afftects the turn on/turn off time.
Part Number: TIDA-00484 Other Parts Discussed in Thread: TPL5111 , TPS61291 , TPS22860 , CC1310
Tool/software:
Hi all,
Basically I use exactly the design as in TIDA-484 with TPL5111, TPS61291 and TPS22860 and I currently, for testing, programmed…
Part Number: TPS22860 Hi Experts, I would like to confirm for SC70 package option. I suppose your team decided to not release SC70 package option. But SC70 package option is still in datasheet page 1. Do you have a plan to develop SC70 package option…
Part Number: TPS22860 Other Parts Discussed in Thread: TPS22950 Hello Experts, My customer is looking for a following load switch. TPS22860 is one of candidate but customer would like to adopt more smaller package. Would you please suggest any devices…
Part Number: TPS22860 Other Parts Discussed in Thread: TPS22916 Hi Sir
When system is off Vin directly to VBAT(3V), ON=low and VBIAS is no power. Can I refer to this parameter below?
And maximum load is 100nA if it is working.
Part Number: TPS22860 Other Parts Discussed in Thread: TPS22810 In a previous forum post , the OP implies they will be connecting 6V to a part with absolute maximum rating for 5.5V.
Due to #ASTOCKALYPSE2021, we have an urgent need to design out TPS27081…
Part Number: TPS22860 Hello Experts, Does this device have a thermal shutdown protection? Also if a current flow through this device exceed 200mA what will be happen? Device will get damage and destroy? (Device will be very hot and will exceed ABS junction…
Part Number: TPS22860 For the part, I have Vin and Vbias measured at 3.3 volts. I have Von also measured at 3.3 volts. I also have attached a 1 uF cap from Vbias to ground, and a 0.1 uF cap from Vout to GND. I followed the layout example from the datasheet…
Part Number: TPS22860 In the datasheet it is written on page 1 that the device is available in the SOT-23 and the SC-70 package.
On page 12 in the ordering information and on the TI website only the SOT-23 package is available.