Part Number: TPS22860 Hi Experts, I would like to confirm for SC70 package option. I suppose your team decided to not release SC70 package option. But SC70 package option is still in datasheet page 1. Do you have a plan to develop SC70 package option or…
Part Number: TPS22860 Other Parts Discussed in Thread: TPS22950 Hello Experts, My customer is looking for a following load switch. TPS22860 is one of candidate but customer would like to adopt more smaller package. Would you please suggest any devices…
Part Number: TPS22860 Other Parts Discussed in Thread: TPS22810 In a previous forum post , the OP implies they will be connecting 6V to a part with absolute maximum rating for 5.5V.
Due to #ASTOCKALYPSE2021, we have an urgent need to design out TPS27081…
Part Number: TPS22860 Hello Experts, Does this device have a thermal shutdown protection? Also if a current flow through this device exceed 200mA what will be happen? Device will get damage and destroy? (Device will be very hot and will exceed ABS junction…
Part Number: TPS22860 Hello,
I have a project where I want to switch a 6V load with a MSP430. I thought I will take two 3V CR2032 and use it in the shown manner. The question is now if the TPS22860 is connected correctly. Or should I rather connect both…
Part Number: TPS22860 In the datasheet it is written on page 1 that the device is available in the SOT-23 and the SC-70 package.
On page 12 in the ordering information and on the TI website only the SOT-23 package is available.
Part Number: TPS22860 Other Parts Discussed in Thread: CC1310 , Hi All,
Hi All,
I would have a technical question for TPS22860 in a board in which I should also use CC1310 as a microcontroller.
This device is battery powered so consumption is crucial. The…
Part Number: TPS22860 Hi,
Please advise us how to calculate "pd - power dissipation".
Could you please let us know the Ron value on Vin=5V? We only find Ron value of Vin=3.3V/2.0V/1.8V.
Thanks and best regards, M.HATTORI.
Part Number: TPS22860 Other Parts Discussed in Thread: TPS22916 Hi Sir
When system is off Vin directly to VBAT(3V), ON=low and VBIAS is no power. Can I refer to this parameter below?
And maximum load is 100nA if it is working.