Part Number: TPS22910A Other Parts Discussed in Thread: TPS2116 Messrs TI,
I am testing a custom board with two TPS22910A devices that share the same output; this is because each of them manages two different power source for the board (USB 5V_EXT &…
Part Number: TPS22910A Hello Team,
My customer is looking for the 3D Step file for the device TPS22910AYZVR. CAn you share this with us?
Thank you in advance
Regards,
Renan
Part Number: TPS22910A Other Parts Discussed in Thread: TPS7A8101 , Hello,
when I download e.g. TPS7A8101 PSpice model I can simulate all nodes, correct? This also works with TPS22910A PSpice model. But when I combine both parts in a new project / schematic…
Part Number: TPS22910A Hello,
I have this device on a new design. Vdd is never removed from the Vin pin. Vin == Vdd == Vbat or 3.3V depending on whether or not the 3.3V boost regulator is enabled. When the regulator in not enabled VBat == Vdd. I am…
Part Number: TPS22910A Hi,
I want to connect this load switch to a RC load with the capacitance value of 10pF. Is it possible to use to this load switch (I need to understand the off capacitance offered by this device) because whenever the switch is…
Part Number: TPS22910A Hi there,
I am interested to find out if the component can be used in Class 2 medical devices.
Also if it is possible, the operating relative humidity (RH) and operating pressure.
Thank you!
Part Number: TPS22910A Hi,
The specs say that the ON pin can not be left floating. In my design I have 3 diodes (anode sides) hooked to the ON pin (which is enabled low). When any of the cathodes of any diode goes to ground, the ON pin drops to ground…
Part Number: TPS22910A Other Parts Discussed in Thread: TIDA-00374 , TPL5110 , , TS5A3160 , TPS22916 Hi,
Referring to TIDA-00374 - looks like a good solution. Though since this a bit dated (May 2016) wondering if there are higher performing replacement…
Part Number: TPS22910A Hi
Could you please tell us your view about the following configuration?
We are about to use TPS22910A for suppressing the leakage from battery.
-On charging TPS22910A : ON state VIN : 4.2V EN : 4.2V VOUT : 4.2V (max)…