Part Number: DRV8210EVM Other Parts Discussed in Thread: TPS22916EVM When I using the other mcu to input high logic level signal into drv8210evm EN/IN1, then I measured the current output from the mcu gpio is 3.44mA average.
I think the current is too…
Hi Amrit,
Customer does not have drafted schematics for this yet, but you can imagine that from the block diagram below, we place LM73100EVM and TPS22916EVM on "Ideal Diode/Load Switch" block.
To create a similar test condition, I have added a resistor…
Hi Stephane,
Was this test performed on an evaluation module?
Using an EVM would be the best way to isolate the device to identify whether it is the source of the leakage.
The evaluation module for this device can be ordered online here: https:…
Part Number: TPS22916 Other Parts Discussed in Thread: , TPS2121 , TPS22917 Hello, I'm going to give some context first so you might understand our situation more easily
We want to design 2 different power management system with some diverse features…
Hi David,
This is not the actual behavior of the device. I believe this may be some artifact of the PSPICE model or of the simulation setup here. I will look into this PSPICE issue but at this time, I was able to confirm RCB behavior with a rising…