Part Number: TPS22917 What is the Counrty of Origin for these parts?
NEED COO FOR THESE PARTS LISTED BELOW PLEASE
5962R9950401VDA
INA240A3DR
TPS7H1121HFT/EM
TPS7H2140MPWPTSEP
5962-8755501VSA
5962R1222403VXC
Part Number: TPS22917 For TPS22917LDBVR During part is enabled EN=0V, and the Vin=3.6V from battery and Vout=Vin When I remove the battery from Vin which has 1M ohm powerdown and the part enabled = 0V and Vout has voltage from super capacitor, the Vin…
Part Number: TPS22917
Tool/software:
Hello, I have three questions.
1. Does RCB (REVERSE CURRENT BLOCKING) work even when the 'ON' pin is disabled? (Von < ViL) The datasheet doesn't clearly state this. (I am leaving a question because I do not fully…
Part Number: TPS22917 Tool/software: Hi TI Team,
We are using TPS22917 in one of our projects, can someone from TI team please review the schematic and let us know the changes if required.
Thanks
Part Number: TPS22917 Hello team,
If ON pin of TPS22917L is connected to GND and Vout is connect to external source, the device is turned on. is this correct?
If yes, in order to active ACB circuit, to block reverse current from external source, 500mA…
Part Number: TPS22917 Other Parts Discussed in Thread: TPS22919 Tool/software: I intend to use the TPS22917 or TPS22919 to disconnect a boost converter (3.3 to 5V).
The question is if it is ok to use the Quick Output Discharge to discarge the output…
Part Number: TPS22917 Other Parts Discussed in Thread: TPS22991 ,
Tool/software:
Hello,
My customer tested the TPS22991 by replacing it with a TPS22917DBVR due to the issue reported in the E2E post below.
RE: TPS22991: Reverse power protection…
Part Number: TPS22917 Hi, TI expert
Can you recommend a LOAD S/W product to turn the 4.2V lithium battery power on/off and supply power to the LTE modem?
The output current is about 1A.
Package SOT23 would be good.
The part I found is TPS22917…