Other Parts Discussed in Thread: TPS22918-Q1 The Bosch UAES R&D wanna get the failure mode and failure rate related material of TPS22918-Q1, please help check it
Thank you!
Part Number: TPS22918-Q1 Other Parts Discussed in Thread: PCA9534A , I saw some of the datasheet like pca9534a indicates the tolerance of the Heigh for the package in the datasheet:
I can calculate the tolerance of high by this diagram. (tolerance = 1…
Part Number: TPS22918 Dear Specialists,
My customer is considering TPS22918 and has questions.
I would be grateful if you could advise.
---
1. I would like to use CT at 0.1u to 0.33u, but the table 1. only shows 0 to 10000p.
Could you please let us know…
Part Number: TPS22918-Q1 Other Parts Discussed in Thread: TPS22918 , Hi Expert,
Thanks a lot for your warm help!
My customer has 2 products in their list,TPS22918 T DBVR Q1 and TPS22918DBVR
The Q1 version is admitted by AEC-Q100.
Except the upper difference…
Part Number: TPS22918 Hi,
I have just confirmed the following.
My customer uses TPS22918 VIN=3.3V. To reducing the board size, is it OK to connect VIN with ON pin directly?
On some case, a few drop on VIN is occurred. But I think ON pin's threshold is…
Part Number: TPS22918 Hi,
On the datasheet P.19, we can find the Inrush Current calculation on Equation (11),(13). But I think both result is wrong. For example Equation(13)'s result (135mA) is wrong, I seem 135nA.
Equation (11) : dt = 22 pF x 4V…
Part Number: TPS22918 Hi,
I have one question.
On the datasheet, we can find the ON pin Hysteresis (Typ. 107mV). Which cases does this apply? ON->OFF case and OFF->ON case?
Please advise us.
Thanks and best regards, M.HATTORI.
Part Number: TPS22918 Hi Team,
Tps22918 is discussed as an application of FPGA power supply sequences.
This time, the power good signal of the other power supply IC (the power supply rise completion signal) is input to the ON pin of TPS22918 to start…