Part Number: TPS22922 Hi Team, May I ask for help? My customer want a transistor part number for his application. He want a transistor switch which can be connected to the battery to stop the battery leakage. His battery voltage is 3.3 v. I am checking TPS22922…
Part Number: TPS22922 Hello Team,
may I ask you to provide the ambient temperature range for TPS22922BYFPR, please?
This is not specified in the data sheet:
Thanks and Best Regards,
Hans
Part Number: TPS22922 Hi support team,
When the input capacitor is 1μF, is the recommended value of the output capacitor 0.1μF?
Or when the output capacitor is 4.7μF, should the input capacitor be 47μF?
Regards, Dice-K
Part Number: TPS22922 I am currently using the TPS22922 load switch in a very simple application where it controls the power to a small altimeter. The input voltage to the load switch is between 2-3V (Coin cell). Input capacitance is >> than the output…
Part Number: TPS22922 Hi Team,
can the ON (EN) Voltage of TPS22922 be higher than the input voltage? So input voltage would be 1.8V and ON would be 3.3V.
Best regards
Simon
Part Number: TPS22995 Other Parts Discussed in Thread: TPS22964C , TPS22922 Hi Team,
I am looking for direct replacement of TCK22975G,LF.
Is there a better fit than TPS22995?
BR, Stefan
Part Number: TPS22922 Hi,
Just checking - suppose i connect the TPS22922 ON pin to 3.3V, then at some point later set VIN to 1.8V. Note this is kind of the opposite of the sequence in its datasheet. Question is, will the part behave correctly i.e. allow…
Other Parts Discussed in Thread: TPS22922 That is the maximum junction temperature for the TPS22922? I see max storage at 150C, max power dissipation (25C ambient) at 645mW, and see the junction to ambient thermal resistance is 131C/W for the YZP package…