Part Number: TPS22924C Please confirm that TPS22924CYZPT does NOT have the backside coating.
It appears that to get the backside coating, one needs to order the larger 3K reel, TPS22924CYZPRB; the "B" suffix appears to imply the backside coating.
…
Part Number: TM4C1231H6PM Other Parts Discussed in Thread: TPS22924C , Hi Team,
We are using TM4C1231H6PM in our design. We are planning to enable 3 TPS22924C ICs with the single GPIO (Pin 6 with 8mA drive strength) from MCU.
Kindly let us know if…
Hi Yuto,
The TPS22924C has a quick output discharge (QOD) feature that keeps VOUT pulled down when the device is not turned on. However, looking at section 9.3.3 in the datasheet, you will see this note:
"The output pulldown is active when the user…
Hi Yuto-san,
There are 2 things missing here:
1. You are missing the output cap.
2. When running the transient sim, please select "Zero Initial Conditions".
This should hopefully resolve your issues.
Other Parts Discussed in Thread: TPS22924C Do you have TPS22924C SOA curve data? I think TPS22924C allow keep 2A current at TA 85degC condition. Is this correct?
Best Regards, Kohei Sasaki
Other Parts Discussed in Thread: TPS22924C , TPS22924 , TPS22925 Please let me know about two points below of TPS22924C.
①About Iin:160μA_max by Datasheet P5, is this spec condition determined for temp range(85℃) and device dispersion?
If it is correct…
Other Parts Discussed in Thread: TPS22924C Pease let me know about 2-point below of TPS22924C.
①About Vout fall time@3.6Vin and Turn-off time@0.9Vin ,
These spec(Typ) are written in Datasheet P5, but "TYPICAL CHARACTERISTICS":P9~P10 are lower than…
Alek-san,
Thank you for your support. I understood that we should add ON signal after Vin becomes high, however there is no guaranteed time characteristic, so we should confirm with actual device operation insted of simulation and decide the delay…
Other Parts Discussed in Thread: TPS22924C Hi
Please let me confirm some questions about relationship between Ron and Output Current.
1:when Output current is increased,How increase is Ron ?
Ex:Regarding to the Datasheet of TPS22924C on page P5…