Other Parts Discussed in Thread: TPS22929D Please let me know the minimum,maximum value of the switching characteristic of TPS22949D.
It is only typical value at the datasheet..
Other Parts Discussed in Thread: TPS22929D Hello
I'm planning to use the TPS22929D part and had a basic question concern the Vih level for the ON pin. If I have 2.5V going into my VIN pin can I drive the ON pin to a 3.3V high. Basically I'm using an…
Part Number: TPS62743 Other Parts Discussed in Thread: TPS22929D , TPS22860
We are experiencing strange behavior with this regulator when we initially turn on the power to our system. I'm happy to share our schematics privately, but I can't share them…
Hi Ed,
Thanks a lot for your reply, and Leonard too.
In fact I did not know this type of component.
I use many IT components, but I always find something new.
I already added the PN TPS22929D in my schematic and I will use a lot.
Thanks a lot guys, …
Other Parts Discussed in Thread: TPS22929D , TPS22918 , TPS22953 , TPS2115A-Q1 , TPS2115A Hi
I have an 5V application with a 0.47 (1ohm ESR) supercapacitor which is used as backup supply when the external supply is disconnected.
During power on, I would like…
Hi Satoshi,
I am moving this thread to the load switches forum, as a load switch with reverse current protection may be sufficient. They would provide the best recommendation, but a quick look at the TPS22910 (61mohm) family and TPS22929D (115mohm) may…
Hi JYL,
It may be simpler to use a load switch with that current carrying capability rather than putting two switches in parallel.
The TPS22929D is a leaded, 5.5V load switch with a current carrying capability of 1.8A. If a WCSP device can be used, then…
Other Parts Discussed in Thread: TPS22929D , TS5A3153 , TPS2113 Hi,
I have 2 sources of Power supply S1 (can be 1.8, 3.3 or 5V) and S2 (always 3.3V). I plan to select voltage between the 2 sources as shown in the following circuit. Also C1 will have to…
Other Parts Discussed in Thread: TPS22929D , TPS27082L , TPS27081A , BQ25504 Hi !
I am planning to use one of the following devices
TPS22929D
TPS27082L
TPS27081A
However, my application will have an inductive load which is different from the datasheet typical…