Part Number: TPS22950 Tool/software: Can you confirm that this is the correct part (TPS22950YBHR) we have installed on our board? The only marking is 41B. See photo.
Thanks.
Part Number: TPS22950 Tool/software: Hi TI Power Switch Guru, I am looking at an alternative for diode + PMOS and thus looking at TPS22950 for an wearable bidirectional charge and discharge application That requires current lim and reverse blocking in…
Part Number: TPS22950 Tool/software: Hi Team
Datasheet as below mention The output voltage is held near zero potential with respect to ground .
but in the figure 9.1 trigger current limit the Vout still under high level voltage
Another question…
Hi Arush,
Thanks for sharing.
Below is the simplified diagram from app note. It seems the MOSFET here is NMOS, but TPS22950-Q1 internal FET is PMOS.
Based on the description in app note, the body diode will block the reverse current. But for PMOS of TPS22950…
Part Number: TPS22950 Tool/software: The Max recommended operating range for Vin is 5.5V. Will exceeding this value (not exceeding the absolute maximum rating of 6V) cause any problems?
Part Number: TPS22950 Tool/software: Hello team,
My customer is trying to estimate the current consumption at the ILIM pin of this device.
How much current would be consumed at ILIM pin? OR What is the voltage of ILIM pin?
Best Regards, Kei Kuwahara
Thanks Tim.
I had received the certification letter of E169910/UL2367, but there is no wording for IEC 62368.
Could you please double confirm whether it is included IEC 62368?
Thanks and Best regards,
Tiger
Part Number: TPS22950 Tool/software: Hi Team
Could you please check the schematics below?
1. Check points (1) Validity of VIN and VOUT capacitance (C302 & C303) (2) ILIM resistance value (R305)
2. Conditions (1)VAUX_1R8V: 1.8V (2) VCCO_3R3V: 3.3V (3)…