Other Parts Discussed in Thread: TPS22951 Hi,
I have some questions about TPS22951 as listed below.
Regarding the value of 600mA current limit value, is there a range of it? What is the minimum value? Is 550mA a reasonable number for our test result? …
Other Parts Discussed in Thread: TPS22951 , TPS22946 Hi all. My customer would like to evaluate TPS22951, but I don't get the EVM of TPS22951. Does this device have EVM? If this device doesn't have EVM, do you have instead of the EVM? Best Regards, …
Hello Sam,
This device does not have short circuit protection. If you turn on this device into a short circuit event that drives the current above its ABS ratings then it can certainly be damaged. If short circuit protection is needed for your system…
Part Number: TPS61222 Other Parts Discussed in Thread: TPS54J060 , TPS22951 Hi, Team,
Now my customer is searching buck DCDC part with the latch protection at overcurrent(Vo shorted to GND).
The spec requested of IC is;
VIN range= max 6V, Programmable VO…
David,
We have /some/ load switches that might work for you as long as your current is <500mA DC.
I would recommend to look at TPS22946 and TPS22951
They have either selectable or fixed current limits and are 5.5V max VIN parts. They are also available…
Part Number: TPS22917 Other Parts Discussed in Thread: TUSB1210 , TPS22953 , TPS22954 , TPS22951 I am using the TUSB1210 with a Zynq XC7Z010. There is good information on sequencing the 1.8V rail for VDD18 and VDDIO after VBAT/VDD33, which is the opposite…
Hi Miriam,
The TPS22951 would be an alternative part here for higher current. would a device like this work? Let me know if you have and idea for how much current the application needs.
Thanks,
Alek Kaknevicius
Part Number: TPS22917 Other Parts Discussed in Thread: TPS22951 , TPS22971 , TPS22990 When the switch is enabled and the QOD output is off (high impedance), what is the leakage current flowing into the QOD pin?
Thanks,
Mark
Hi Vikas,
Rakesh has provided some of our best alternative options since the TPS2294x devices and TPS22951 are our only current limited load switches with flag pins. The only other current limited and fault reporting devices we have are our eFuses, and you…