Part Number: TPS22954 Hi Sir,
What is the tolerance(min&max) of this rise time? Is there a condition of VIN=2.5V that can be provided?
Is the discharge time in the figure the waveform of TPS22964? If not, discharge waveform of TPS22964 that can be…
Part Number: TPS22954 Hello everyone.
I use this power switch to feed a resistive load connected through very long wire - basically an LR load.
During shutdown via the EN pin, the switch needs to discharge the energy in the wire's inductance. Because…
Part Number: TPS22954 Other Parts Discussed in Thread: LM3881 Hi Team,
My customer is planning on using our LM3881 to power the enable pin of the TPS22954. A concern of my customer is that the TPS22954 may turn on due to the Vflag votlage ramping up as…
Part Number: TPS22954 Other Parts Discussed in Thread: TPS22953 Hello,
I am planning to use TPS22954 (with QOD) in my design , currently using TPS22953 & planning to replace with TPS22954.
My Bias voltage will drop to 1.5 V from 3.3 V when the enable…
Part Number: TPS22954 Datasheet page-24 is described that unused PG pin is tie to GND.
About unused PG, I think that left open is no problem, is it correct?
Best regards,
Satoshi
Other Parts Discussed in Thread: TPS22954 Is TPS22954 require to control power off sequence for Vbias and Vin?
(Power up sequence is no require)
Best regards,
Satoshi
Other Parts Discussed in Thread: TPS22954 , TPS22953 , TPS2420 , TPS2421-2 Hi,
Can someone tell me the difference between TPS22954 and TPS22953? Also, does TI have any current limiting load switches with Power Good feature?
Thanks!
Hi User,
Not exactly, we do have devices that have one enable pin and one reference pin that can be used to externally trigger a fault/shutdown condition. A good example of this is TPS22953 and TPS22954. https://www.ti.com/lit/ds/symlink/tps22953.pdf …
Hi Delaney,
I believe you are looking for some form of UVLO. Unfortunately, TPS22990 does not have integrated UVLO like devices such as TPS22810, TPS22953 and TPS22954.