Part Number: TPS22958 Hello Expert,
We have a TPS22958DGN on multiple of our boards, but the chips do not seem to fully turn off. Even with the ON pin held low, there is still a steady voltage level on the output. The DGN version should have the QOD…
Part Number: TPS22958 Tool/software: Hi,
I expect to use TPS22958DGNR as the load switch to cut the connection between a 1-cell Li-Ion Battery and a BMS circuit for one of my projects.
When the battery is up for charging, the supply/main current should…
Part Number: TPS22958 Other Parts Discussed in Thread: TPS2116 , TPS22916 Hello,
I am working on a PCB design that features 2 SFP+ ports that will host SFP+ transceiver modules with extended range operating temps from -40C to +85C. Each SFP+ module…
Part Number: TPS22958 Other Parts Discussed in Thread: TPS22992 I need 3A @ 5V so 15W. The total current is 6A which is fine, and it can operate at 5V, but doesn't mean I'm going to get that much out of it in reality. I don't see in the datasheet where…
Hi,
sorry, i didn't see the question as the thread was marked resolved.
If you want to measure the leakage from just one channel to output, it shouldn't matter if the other channels are completely floating, as i don't think there is a potential…
Part Number: TPS22958 Hello TI forum.
The load switch will usually not work. But sometimes after trying a lot, it will start working. And then it might work for a little bit and then suddenly stop working. I have replaced the part twice now on two different…
Part Number: TPS22958 Hi
Can I PWM the ON pin to control the output voltage?
If not is there a load switch available which I can use in such a way?
Thanks in Advance
Part Number: TPS22958 Hi,
TPS22958NDGNR is a device with Thermal pad, the dimension of thermal pad is not specified in the datasheet. Please share the same for creating the footprint
Part Number: TPS22958 Other Parts Discussed in Thread: TPS22917 , TPS22916 , TPS2663 Hi <
Do TPS22958 block the reverse current from the O/P to I/P ?
Do you have a similar device which can switch Voltages from 4 V to say 40 V with a min 3 A Capability…