Part Number: TPS22960EVM Other Parts Discussed in Thread: TPS22960 , TPS22963C Hi In the above schematic I have used TPS22960 switches for connecting different voltages. But when I am disabling all the voltage sources and connecting external pullup the…
Other Parts Discussed in Thread: TPS22960 , CC1120
Hello all,
We use TPS22960 at our new design but there is an unexpected state.
VIN1 = 2.7V
VIN2 = 3.6V
When both control inputs are low, Vout1 = 0.707V, Vout2 = 0V and almost 20mA current consumption…
Part Number: TPS22960 Other Parts Discussed in Thread: CC2650 Hi
I am facing problem with power switch TPS22960 output voltage zero for Input voltage 3.0 volt and ON1 and ON2 pin both are High (3.0V )
The voltage at VOut 1 is 2.5V and VOut 2 voltage…
Part Number: TPS22966 Other Parts Discussed in Thread: TPS22960 Hi,
I would like to use two different voltage levels at Vin1 and Vin2. Can Vbias be constant irrespective of Vin?
Other Parts Discussed in Thread: TPS22960 Dear All.
one customer working on VTS(vechile tracking system) . he requesting following details
TPS22960 Peak Current.
it is not mention in the datasheet
RDS
Rajesh
Other Parts Discussed in Thread: OPA1662 , OPA1664 , TPS22919 , TPS22960 , TLV702 , TLV7021 , TLV702-Q1 Hello,
I recently designed a PCB using some TI components. I wasted to perform a signal and power integrity analysis of the PCB. I needed the IBIS models…
Hi Lucas,
Please refer to https://www.ti.com/power-management/power-switches/load-switches/products.html to view our load switch catalog.
Using the filters, you are able to select 2 channel devices. I would suggest looking at TPS22960 or TPS22968. I think…
Hi Vikas,
Thanks for reaching out!.
Clearly understand your requirement of low Iq, non BGA and protection against external faults. But unfortunately, we don't have device which matches your requirements. The closet I see are load switches TPS22917, TPS22960…