Part Number: TPS22962 Other Parts Discussed in Thread: TPS22965 , Hi TI Team,
We are using the following two load switches in our design:
TPS22965DSGT
TPS22962DNYR
As per the datasheets, VIN must be less than or equal to VBIAS.
Could you…
Part Number: TPS22962 Hello,
My customer wants to use a pull-down resistor on the ON pin of the TPS22962.
What is the appropriate resistance value and how to determine it?
Thank you.
JH
Part Number: TPS22962 Other Parts Discussed in Thread: TPS22959 , Can the load switch(tps22962 and tps22959) be controlled by an ON voltage of 0.85V under(Vbias=5V,Vin=0.85V,Vout=0.85V)
If not what is the minimum ON voltage?
Part Number: TPS22962 Hi,
Please review my design of TPS22962 and let me know if you have any comments.
Vin = 3.3V
Vbias=3.3V
ON=3.3V from PGOOD of a regulator
The 9th pin is Thermal pad connected to VIn
Please let me know your review…
Part Number: TPS22962 Other Parts Discussed in Thread: TPS22953
Hi, Customer is considering the TPS22962 in the following configuration. Is it a problem that 5 V is added to Vout on the SW2 side in SW2 disable condition? Customers want to know the risk…
Hi Yash,
I think the issue may be your PAD connection. In the schematic, you have it connected to GND, but this is actually a connection for VIN. This would affect the voltage at VIN and prevent the 5V from reaching the output.
Thanks,
Alek Kak…
Hi Massimiliano,
I went down into the lab and took some measurements using the TPS22962:
VIN = 1.2V, VBIAS = 3.3V, COUT = 0.1uF, RLOAD = 10Ω
Temperature (°C)
Delay Time (us)
Rise Time (us)
Fall Time (us)
-40
723
677
2
…
Thanks Gerold, any idea when the webench will be updated?
We are not very familiar with Pspice model, so we have some trouble to create the project in hyperlinx and link it to the Pspice model of the TPS22962.
I wonder why the webench project didn…
Part Number: TPS22990 Other Parts Discussed in Thread: TPS22962 , TPS25985 Tool/software: Dear team,
Can two TPS22990 or TPS22962 working in parallel like below? the output and inputs tied together:
Thanks,
Charles
Part Number: TPS22969 Other Parts Discussed in Thread: TPS22959 , , TPS22962 Hi support team.
I have received some questions from my customers regarding TPS22969, TPS22962 and TPS22959 as described below.
1. Since the three products differ only in…