Part Number: TPS22963C
Hi,
I was using the Ic's TPS22963C(to generate VCCAUX_1V8 from 1V8)and TPS7A8300RGWT (to generate VMGTAVCC_1V and VMGTAVTT_1.2V from 1V8).The EN pin (of TPS7A8300RGWT) and the ON pins (of TPS22963C) were driving from the…
Part Number: TPS22963C Other Parts Discussed in Thread: TPS22960 Can we connect TPS22963C switches in parallel. When ever the switch is disabled will it ground the line. And some times I want to connect a external source at the output of the switch will…
Part Number: TPS22963C Hi there,
As title, what happens when the ON pin voltage of TPS22963C is between the VIH and VIL operating range?
Thank you!
Best regards,
Roy Hsu
Part Number: TPS22963C Hi Expert,
If the VBUS_CHGR_USB didn't have power in, but VOUT has the power. Does it any risk that VIN get the power Vout? Because C2 pin didn't connect to GND. Thanks!
Part Number: TPS22963C Hi, Could you tell me about TPS22963C data sheet page 17,18? The following contents are described in the data sheet page 17. I do not understand the meaning of "Maximum Acceptable Inrush Current". Please tell me in more detail…
Other Parts Discussed in Thread: TPS22963C Hi Team,
I couldn't find it listed on the datasheet, but what voltages do the load switch turn on and turn off? For example:
if my GPIO logic levels are at 3.3, and I'm enabling a 1.8V load, since Venable…
Hi Stefan
The TPS22925 is p2p to the TCK22975G, and it has a higher current rating with lower resistance. The only deviation is that it is active high instead of active low.
Please see TPS22963C /TPS22964C (no QOD/QOD) and TPS22921 /TPS22922 (no QOD/QOD…
“In our application, in one case, this device will not have power (VIN=0) and enable will low.
But there will be 5V present at the output. Will reverse current protection work in this mode?
Will this device be damaged if 5V is present at output…
Part Number: TPS22964C Other Parts Discussed in Thread: TPS22953 , , TPS22963C Hi Team,
I found in the data sheet of TPS22953 application note in the data sheet (page 32, 10.1.6 section) connection of 2 parts of TPS22953 with 2 USB inputs and one output…
Hi Shreyas,
Thanks for your reply. That is very helpful. I want to make sure that a part (e.g., TPS22963C: reverse current protection when disabled) have the same low Ron for either Vin>Vout or Vin<Vout. So that I will be able to run any value of continuous…