Part Number: TPS22965 Hi
The customer is concerned that the maximum Tj of TI's TPS22965 is lower than that of the existing AX8760 and would like to confirm whether there are any thermal risks under high ambient temperature conditions.
Although the…
Part Number: TPS22965-Q1 Good morning. Why does the blue trace (VOUT) start ramping up (circled in the photo) before the ON command (yellow trace) is activated? It appears to start at 50% of Vin. Thank you best regards, Angelo.
Part Number: TPS22965 May I know what is the COD of #TPS22965DSGR and #TPS61021ADSGR?
#TPS22965DSGR
LOT code
6062848CL6
#TPS61021ADSGR
LOT code
5475819CD5
Part Number: TPS22965 HI TEAMs
Currently, we plan to use the TPS22965 for VDD control of the LCD screen. During the power-on and power-off sequence operations of the LCD screen, the power-on (ON) of the LCD works without issues. However, the LCD datasheet…
Part Number: TPS22965-Q1 Hi team,
Can you provide the ON-state resistance info for the TPS22965-Q1 at VBIAS=3.3V? The datasheet only has info for VBIAS=5V and 2.5V.
BR,
Daniel
Part Number: TPS22965 What is the maximum load capacitance that the TPS22965QWDSGRQ1 should be connected to. I do not see any maximum load capacitance stated, but the load mentioned several times is in the range of 0.1 uF to 22 uF.
In my case, the…
Part Number: TPS22965 Other Parts Discussed in Thread: TPS22953 Tool/software: Hello TI Experts ,
Section 10.1.3 of the TPS22965 datasheet indicates that a Cin greater than CL is highly recommended due to the current flow through the body diode from…
Part Number: TPS22965 Hello TI team,
Please support to provide the PPAP readiness timeline for the below part along with the Years to EOL details.
TPS22965NQWDSGRQ1.
Thanks & Regards,
Megha