Part Number: TPS22965 Hello,
My customer and I are trying to figure out how to properly calculate rise time for this part based off of the datasheet. Looking at the slew rate equation 1 in the datasheet, it does not match up with the rise times shown…
Part Number: TPS22965 Found that the MSL label on the physical and MSL indicate in datasheet is difference.
Kindly advise which is the correct MSL for MPN# TPS22965NDSGR.
What is the reason causing difference MSL?
Part Number: TPS22965 Other Parts Discussed in Thread: TPS1641 , LM74202-Q1 Tool/software: Hi
Could you help suggest a LOAD SWITCH with a withstand voltage of 32V or above, a current of 0.5A, and a VCC of 3V to operate. Automotive standards are also…
Part Number: TPS22965-Q1 Tool/software: Hello Team,
In Our design we are using TPS22965QWDSGTQ1 IC, Can you let us know with your feedback
Regards,
Tirthal Patel
Part Number: TPS22965-Q1 Tool/software: Hey all,
I've got a question on acceptable input voltage, below would be my target implementation:
Vin = 3.3V
Vout = 3.3V
EN = 5V
Vbias = 5V
Are these acceptable? Is there a path from EN to VIN if…
Part Number: TPS22965 Tool/software: Hello Team,
Could you please let us know if we can choose option1 or option2 for side wall metal thickness?
I think this options come from difference of assembly site. Is that correct?
Best regards, …