Part Number: TPS22965-Q1 Dear team,
Before ON pin pulls high, we found that there is 1.4V output, and the input is 0.7V. Due to PMIC's BIST mode, VIN has a 0.7V leakage voltage. But we don't know why 22965's output has a larger leakage output. Could you…
Part Number: TPS22965-Q1 Hi, I Intend to use the TPS22965NQWDSGTQ1 load switch as part of the power sequencer circuit. There are 2 types switching 3.3V, and 1.8V. I do not have 5V power in my card and I want to be sure that I can have my circuit without…
Part Number: TPS22965-Q1 Other Parts Discussed in Thread: ADC128S052-Q1 Hello,
We are using the ADC "TPS22965-Q1" via SPI.
We wanted to know if you could support us with a sample code.
Also, an example with higher sampling frequency will be…
Part Number: TPS22965-Q1 Other Parts Discussed in Thread: TPS22965 , We use TPS22965 (-40+85 ) that support 6A in an application with MAX temp +85°C and theorically can consume up to 6A. This P/N unfortunately is not available until the end 2022. Maybe…
Part Number: TPS22965-Q1 Hi team,
My customer is trying to select which one to order for evaluation. But from out package information and device comparison table, we don't know how to recognize right part number.
So could you help us to point out…
Part Number: TPS22965-Q1 Dear team,
When testing our device, my customer found that the TPS22965-Q1's output is abnormal. After being enabled, our device's output is 1.8V, after 1.33 seconds, the output becomes normal 3.3V. The input of our device is…
Part Number: TPS22965-Q1 Other Parts Discussed in Thread: TPS22965 , TPS22990 Slew Rate Capacitor (Ct) to be chosen in TPS22965 (n-load Switch), The Load Capacitance is about 162uF for our Design. We can not maintain Cin/Cload ratio of 10:1 as per datasheet…
Part Number: TPS22995H-Q1 Other Parts Discussed in Thread: TPS22965-Q1 I need to implement a High-Power (0.5A) Bus-Powered Device (Function).
From what I understand, the Host and Device will initially enumerate, up to 100mA. I will keep the VBUS load…