Part Number: TPS22966-Q1 Tool/software: Based on the schematic diagram of TPS22966TDPURQ1, The maximum current of the two outputs does not exceed 200mA. Can you please check if the design is reasonable? If you have any questions, please explain and provide…
Part Number: TPS22966-Q1 Hi team,
Would you please check if I don't use channel 2, can I just leave VIN2/ON2/VOUT2/CT2 floating?
Or I should connect ON2 to ground, and leave VIN2/VOUT2/CT2 floating?
Thank you.
Regards,
Allen
Part Number: TPS22976 Other Parts Discussed in Thread: TPS22966 Hi Team,
Does the VOUT1 and VOUT2 of TPS22976 be connected together to combine to output 12A current? Customer project requirements must support 8A.Can TPS22976 support combine to support…
Part Number: TPS22966 Hello Team,
If one of the channels for TPS22966 needs to go unused would it be better to ground both sides or leave both sides floating?
Best Regards,
Casey
Part Number: TPS22966 Hi
My Customer has question.
Is it OK even if CT1 and CT2 of TPS22966 are common and mounting one capacitor?
Customers want to make the mounting area as small as possible.
Best Regard
T Kishi
Part Number: TPS22966-Q1 Other Parts Discussed in Thread: TPS22966 Hi
My Customer has question.
[TPS22966-Q1] has higher ESD (HBM) than [TPS22966]. Is the Diode for ESD different?
The customer wants the ESD of [TPS22966 - Q 1] to be stronger than [TPS22966…
Part Number: TPS22966 Hi
My Customer has question.
Customers wish to use TPS 22966 as a measure against hot plugin.
TPS22966.pdf
・It will be connected in the order of GND => VIN 1 and VIN 2. ・While the pad terminal is sliding there is a possibility…
Part Number: TPS22966 Other Parts Discussed in Thread: TPS22990 , Hi all,
I have a problem in using TI's TPS22966DPUT. The VCCINT_A is controlled by TPS22990, and the control signal is FPGA_EN. After starting up, FPGA_EN is pulled high in the start…