Part Number: TPS22966-Q1 Hi,
Im an AE for the USB gruop, and I'm looking for a Vbus switch that has fault detection built in.
I need the switch be rated for 5V 4A-6A with an error detect signal.
The TPS22996-Q1 has the rating I need, but does not…
Part Number: TPS22966-Q1 I am using TPS22966TDPURQ1 as a 1.8V load switch, please find the below waveform capture for input and output supply through TPS22966TDPURQ1 part and schematic design as well. Please let me know if this is the expected behavior…
Hi Shreyas,
Thanks for the feedback! This is noted. Is that why also the slew rate is also different? Even if the TPS22966 and TPS22966-Q1 have the same Slew Rate equation? Our customer also noticed that the Rise Time value is not close to one another…
Part Number: TPS22966-Q1 Hi team,
Would you please check if I don't use channel 2, can I just leave VIN2/ON2/VOUT2/CT2 floating?
Or I should connect ON2 to ground, and leave VIN2/VOUT2/CT2 floating?
Thank you.
Regards,
Allen
Part Number: TPS22966-Q1 Other Parts Discussed in Thread: TPS22966 Hi
My Customer has question.
[TPS22966-Q1] has higher ESD (HBM) than [TPS22966]. Is the Diode for ESD different?
The customer wants the ESD of [TPS22966 - Q 1] to be stronger than…
Part Number: TPS22966-Q1 Tool/software: Based on the schematic diagram of TPS22966TDPURQ1, The maximum current of the two outputs does not exceed 200mA. Can you please check if the design is reasonable? If you have any questions, please explain and provide…
Hi Jiang,
Thanks for reaching out on E2E and being patient as many of us are returning from holidays! Happy Holidays!
The TPS22966-Q1 is an older device, we don't generate SOA curves for other load switches including the TPS22968-Q1.
The SOA curve…
Hi Ryuji,
Have you taken a look at the TPS22966-Q1? This is a dual channel device with each channel rated for 4A. By putting the two channels in parallel, the device would be able to handle the 4.4A load at 1V. Would this solution be acceptable for…
Hi Vishal,
Would you be able to provide a bit more information on this application? Specifically, if the input supply is 2.5V @20A then why does the solution need to handle >30A?
While some of our load switches offer reverse current protection, none…
Hi Tateo,
Let me answer some of your questions one at a time:
1. They want to make sure about the meaning of Ipls rating. Does this adopt for continuous pulse? In other words which means 15msec period and 300usec 6A peak pulse(pulse<300us,2% duty…